WideString Class¶
-
class
NXOpen.UIStyler.
WideString
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a WideString for UI Styler
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ItemValue | Returns or sets the string value for this dialog item. |
Sensitivity | Returns or sets the sensitivity of the wide string |
Visibility | Returns or sets the visibility of the wide string |
Methods¶
Method | Description |
---|---|
AddActivateHandler | Registers activate callback. |
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
InitializeAttachment | Returns initialized dialog item attachment information |
IsEqualTo | Equates two styler items |
SetAttachment | Specifies the updated dialog item attachment information |
SetFocus | Indicates that this dialog item is receiving keyboard focus. |
SetLabel | Specifies descriptive text to display for the dialog item. |
Property Detail¶
ItemValue¶
-
WideString.
ItemValue
¶ Returns or sets the string value for this dialog item.
It can be the initial value that is programmatically defined, or interactively entered by the user.
-------------------------------------
Getter Method
Signature
ItemValue
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ItemValue
Parameters: itemValue (str) – New in version NX5.0.0.
License requirements: None.
Sensitivity¶
-
WideString.
Sensitivity
¶ Returns or sets the sensitivity of the wide string
-------------------------------------
Getter Method
Signature
Sensitivity
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sensitivity
Parameters: type (bool) – New in version NX5.0.0.
License requirements: None.
Visibility¶
-
WideString.
Visibility
¶ Returns or sets the visibility of the wide string
-------------------------------------
Getter Method
Signature
Visibility
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility
Parameters: type (bool) – New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddActivateHandler¶
-
WideString.
AddActivateHandler
¶ Registers activate callback.
This method should be called before calling
UIStyler.Dialog.Show()
orUIStyler.Dialog.RegisterWithUiMenu()
Signature
AddActivateHandler(activateevent, isDialogLaunchingEvent)
Parameters: - activateevent (CallableObject) –
- isDialogLaunchingEvent (bool) –
New in version NX5.0.0.
License requirements: None.