Toggle Class¶
-
class
NXOpen.UIStyler.
Toggle
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a Toggle for UI Styler.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ItemValue | Returns or sets an item value |
Visibility | Returns or sets the visibility of the toggle |
Methods¶
Method | Description |
---|---|
AddValueChangedHandler | Registers value change callback. |
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
GetSensitivity | Gets the sensitivity |
InitializeAttachment | Returns initialized dialog item attachment information |
IsEqualTo | Equates two styler items |
SetAttachment | Specifies the updated dialog item attachment information |
SetDefaultAction | Indicates that this dialog item should override the accelerator on the second mouse button, which normally accelerates to the OK button. |
SetFocus | Indicates that this dialog item is receiving keyboard focus. |
SetLabel | Sets the label to display on the right side of the toggle button. |
SetSensitivity | Sets the sensitivity of the toggle button |
Property Detail¶
ItemValue¶
-
Toggle.
ItemValue
¶ Returns or sets an item value
-------------------------------------
Getter Method
Signature
ItemValue
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ItemValue
Parameters: itemVal (bool) – New in version NX5.0.0.
License requirements: None.
Visibility¶
-
Toggle.
Visibility
¶ Returns or sets the visibility of the toggle
-------------------------------------
Getter Method
Signature
Visibility
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility
Parameters: type (bool) – New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddValueChangedHandler¶
-
Toggle.
AddValueChangedHandler
¶ Registers value change callback.
This method should be called before calling
UIStyler.Dialog.Show()
orUIStyler.Dialog.RegisterWithUiMenu()
Signature
AddValueChangedHandler(valuechangedevent, isDialogLaunchingEvent)
Parameters: - valuechangedevent (CallableObject) – Value changed event
- isDialogLaunchingEvent (bool) – True if launch any dialog else False
New in version NX5.0.0.
License requirements: None.
GetSensitivity¶
-
Toggle.
GetSensitivity
¶ Gets the sensitivity
Signature
GetSensitivity()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
SetDefaultAction¶
-
Toggle.
SetDefaultAction
¶ Indicates that this dialog item should override the accelerator on the second mouse button, which normally accelerates to the OK button.
When you set this attribute, a click on the second mouse button triggers this dialog item’s ON/OFF state and calls the Value Changed callback instead of the action of the OK button.
Signature
SetDefaultAction()
New in version NX5.0.0.
License requirements: None.
SetFocus¶
-
Toggle.
SetFocus
¶ Indicates that this dialog item is receiving keyboard focus.
Signature
SetFocus()
New in version NX5.0.0.
License requirements: None.