TabControl Class¶
-
class
NXOpen.UIStyler.
TabControl
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a Tab Control for UI Styler.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
PageSwitchData | Returns the page switch data |
Sensitivity | Returns or sets the sensitivity of the dialog item |
Visibility | Returns or sets the visibility of the dialog item |
Methods¶
Method | Description |
---|---|
AddSwitchHandler | Registers switch callback. |
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
InitializeAttachment | Returns initialized dialog item attachment information |
IsEqualTo | Equates two styler items |
SetAttachment | Specifies the updated dialog item attachment information |
SetFocus | Sets focus |
Property Detail¶
PageSwitchData¶
-
TabControl.
PageSwitchData
¶ Returns the page switch data
-------------------------------------
Getter Method
Signature
PageSwitchData
Returns: Return type: NXOpen.UIStyler.PageSwitchData
New in version NX5.0.0.
License requirements: None.
Sensitivity¶
-
TabControl.
Sensitivity
¶ Returns or sets the sensitivity of the dialog item
-------------------------------------
Getter Method
Signature
Sensitivity
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sensitivity
Parameters: type (bool) – TRUE if sensitive, FALSE if insensitive New in version NX5.0.0.
License requirements: None.
Visibility¶
-
TabControl.
Visibility
¶ Returns or sets the visibility of the dialog item
-------------------------------------
Getter Method
Signature
Visibility
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility
Parameters: type (bool) – TRUE if visible, FALSE if invisible New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddSwitchHandler¶
-
TabControl.
AddSwitchHandler
¶ Registers switch callback.
This method should be called before calling
UIStyler.Dialog.Show()
orUIStyler.Dialog.RegisterWithUiMenu()
Signature
AddSwitchHandler(switchevent, isDialogLaunchingEvent)
Parameters: - switchevent (CallableObject) –
- isDialogLaunchingEvent (bool) –
New in version NX5.0.0.
License requirements: None.