Separator Class¶
-
class
NXOpen.UIStyler.
Separator
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a Separator for UI Styler
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Visibility | Returns or sets the visibility of the separator |
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
InitializeAttachment | Returns initialized dialog item attachment information |
IsEqualTo | Equates two styler items |
SetAttachment | Specifies the updated dialog item attachment information |
Property Detail¶
Visibility¶
-
Separator.
Visibility
¶ Returns or sets the visibility of the separator
-------------------------------------
Getter Method
Signature
Visibility
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility
Parameters: type (bool) – New in version NX5.0.0.
License requirements: None.