PushButton Class¶
-
class
NXOpen.UIStyler.
PushButton
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a PushButton for UI Styler
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Sensitivity | Returns or sets the senstivity of dialog. |
Visibility | Returns or sets the visibility of dialog. |
Methods¶
Method | Description |
---|---|
AddActivateHandler | Registers activate callback. |
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
InitializeAttachment | Returns initialized dialog item attachment information |
IsEqualTo | Equates two styler items |
SetAttachment | Specifies the updated dialog item attachment information |
SetBitmap | Specifies a filename that contains a bitmap definition. |
SetDefaultAction | Sets default action |
SetFocus | Indicates that this dialog item is receiving keyboard focus. |
SetLabel | Specifies descriptive text to display for the dialog item. |
Property Detail¶
Sensitivity¶
-
PushButton.
Sensitivity
¶ Returns or sets the senstivity of dialog.
-------------------------------------
Getter Method
Signature
Sensitivity
Returns: senstivity of dialog Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sensitivity
Parameters: type (bool) – to set senstivity of dialog New in version NX5.0.0.
License requirements: None.
Visibility¶
-
PushButton.
Visibility
¶ Returns or sets the visibility of dialog.
-------------------------------------
Getter Method
Signature
Visibility
Returns: to get visibility of dialog Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility
Parameters: type (bool) – to set visibility of dialog New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddActivateHandler¶
-
PushButton.
AddActivateHandler
¶ Registers activate callback.
This method should be called before calling
UIStyler.Dialog.Show()
orUIStyler.Dialog.RegisterWithUiMenu()
Signature
AddActivateHandler(activateevent, isDialogLaunchingEvent)
Parameters: - activateevent (CallableObject) –
- isDialogLaunchingEvent (bool) –
New in version NX5.0.0.
License requirements: None.
SetBitmap¶
-
PushButton.
SetBitmap
¶ Specifies a filename that contains a bitmap definition.
The filename must contain a UBM, XPM, or BMP extension. When you use this field, the system displays a bitmap for this dialog item instead of a text label. When a bitmap is present, the system uses the text label as a popup hint when a user places the mouse cursor over the bitmap.
Signature
SetBitmap(bitmap)
Parameters: bitmap (str) – the bitmap extension New in version NX5.0.0.
License requirements: None.
SetDefaultAction¶
-
PushButton.
SetDefaultAction
¶ Sets default action
Signature
SetDefaultAction()
New in version NX5.0.0.
License requirements: None.
SetFocus¶
-
PushButton.
SetFocus
¶ Indicates that this dialog item is receiving keyboard focus.
Signature
SetFocus()
New in version NX5.0.0.
License requirements: None.
SetLabel¶
-
PushButton.
SetLabel
¶ Specifies descriptive text to display for the dialog item.
It should describe the dialog item’s intended use. If you specify a bitmap for this dialog item, it uses this text as tooltip text.
Signature
SetLabel(strLabel)
Parameters: strLabel (str) – the label string New in version NX5.0.0.
License requirements: None.