Properties¶
Property | Description |
---|---|
ItemValue | Returns or sets the item value |
Visibility | Returns or sets the visibility |
Methods¶
Method | Description |
---|---|
AddActivateHandler | Registers activate callback. |
Dispose | Free resources associated with the instance. |
GetBitmap | Returns an array of bitmaps |
GetItemType | Gets the dialog item type. |
GetItems | Returns an array if items |
GetSensitivity | Gets the sensitivity |
InitializeAttachment | Returns initialized dialog item attachment information |
IsEqualTo | Equates two styler items |
SetAttachment | Specifies the updated dialog item attachment information |
SetBitmap | Set an array of bitmap filenames |
SetItems | Set an array of items |
SetLabel | Sets label |
SetSensitivity | Sets the sensitivity |
Property Detail¶
ItemValue¶
-
OptionMenu.
ItemValue
¶ Returns or sets the item value
-------------------------------------
Getter Method
Signature
ItemValue
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ItemValue
Parameters: subitemIndex (int) – Zero-based index indicating the choice to be selected. It must be in the range of existing choices. New in version NX5.0.0.
License requirements: None.
Visibility¶
-
OptionMenu.
Visibility
¶ Returns or sets the visibility
-------------------------------------
Getter Method
Signature
Visibility
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility
Parameters: type (bool) – TRUE if visible, FALSE if invisible New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddActivateHandler¶
-
OptionMenu.
AddActivateHandler
¶ Registers activate callback.
This method should be called before calling
UIStyler.Dialog.Show()
orUIStyler.Dialog.RegisterWithUiMenu()
Signature
AddActivateHandler(activateevent, isDialogLaunchingEvent)
Parameters: - activateevent (CallableObject) – Callback for activate event
- isDialogLaunchingEvent (bool) – TRUE if dialog is going to launch, FALSE if not
New in version NX5.0.0.
License requirements: None.
GetBitmap¶
-
OptionMenu.
GetBitmap
¶ Returns an array of bitmaps
Signature
GetBitmap()
Returns: Return type: list of str New in version NX5.0.0.
License requirements: None.
GetItems¶
-
OptionMenu.
GetItems
¶ Returns an array if items
Signature
GetItems()
Returns: Return type: list of str New in version NX5.0.0.
License requirements: None.
GetSensitivity¶
-
OptionMenu.
GetSensitivity
¶ Gets the sensitivity
Signature
GetSensitivity()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
SetBitmap¶
-
OptionMenu.
SetBitmap
¶ Set an array of bitmap filenames
Signature
SetBitmap(bitmaps)
Parameters: bitmaps (list of str) – An array of one or more bitmap filenames. If all bitmaps for the option menu reside in the same file, specify an array of just one entry, which contains the bitmap filename for this attribute. All existing choices for the option menu remains intact when this attribute is set. Only the bitmaps are changed. Note that the number of bitmaps must match the number of existing choices. New in version NX5.0.0.
License requirements: None.
SetItems¶
-
OptionMenu.
SetItems
¶ Set an array of items
Signature
SetItems(strListArray)
Parameters: strListArray (list of str) – An array of new choices to be used for the dialog item. Note that this removes all existing choices (both text and bitmaps) New in version NX5.0.0.
License requirements: None.
SetLabel¶
-
OptionMenu.
SetLabel
¶ Sets label
Signature
SetLabel(strLabel)
Parameters: strLabel (str) – Text to be set for the descriptive label. New in version NX5.0.0.
License requirements: None.
SetSensitivity¶
-
OptionMenu.
SetSensitivity
¶ Sets the sensitivity
Signature
SetSensitivity(subitemIndex, type)
Parameters: - subitemIndex (int) – If the entire dialog item should change to the new Sensitivity state, set this field to UF_STYLER_NO_SUB_INDEX. If only one subitem should change to the new sensitivity state, set this field to its zero-based index.
- type (bool) – TRUE if sensitive, FALSE if insensitive
New in version NX5.0.0.
License requirements: None.