MultiSelectList Class¶
-
class
NXOpen.UIStyler.
MultiSelectList
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a MultiSelectList for UI Styler
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Sensitivity | Returns or sets the senstivity |
Visibility | Returns or sets the visibility |
Methods¶
Method | Description |
---|---|
AddActivateHandler | Called when a dialog user selects an entry with a double mouse click or presses Return on a selected item. |
AddDoubleClickHandler | Registers double click callback. |
Append | Appends one or more entries to be inserted into the list |
DeleteSubitem | Deletes sub item |
Deselect | Requests a list entry to be deselected. |
Dispose | Free resources associated with the instance. |
Focus | Indicates that this dialog item is receiving keyboard focus. |
GetAllIndicesSelected | Gets the indices of all selected list entries. |
GetAllNameSelected | Gets the names of all selected list entries. |
GetItemType | Gets the dialog item type. |
GetListItems | Gets an array of character strings for item names that are used as selectable choices for this dialog item. |
InitializeAttachment | Returns initialized dialog item attachment information |
InsertSubitems | |
IsEqualTo | Equates two styler items |
SetAllSelected | Specifies all list entry to be selected. |
SetAttachment | Specifies the updated dialog item attachment information |
SetListItems | Specifies an array of character strings for item names that are used as selectable choices for this dialog item. |
SetSelected | Specifies particular list items to be selected. |
ShowSubItem | Requests a list entry to be scrolled up to the first line in the list |
Property Detail¶
Sensitivity¶
-
MultiSelectList.
Sensitivity
¶ Returns or sets the senstivity
-------------------------------------
Getter Method
Signature
Sensitivity
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sensitivity
Parameters: type (bool) – New in version NX5.0.0.
License requirements: None.
Visibility¶
-
MultiSelectList.
Visibility
¶ Returns or sets the visibility
-------------------------------------
Getter Method
Signature
Visibility
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility
Parameters: type (bool) – New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddActivateHandler¶
-
MultiSelectList.
AddActivateHandler
¶ Called when a dialog user selects an entry with a double mouse click or presses Return on a selected item.
Signature
AddActivateHandler(activateevent, isDialogLaunchingEvent)
Parameters: - activateevent (CallableObject) –
- isDialogLaunchingEvent (bool) –
New in version NX5.0.0.
License requirements: None.
AddDoubleClickHandler¶
-
MultiSelectList.
AddDoubleClickHandler
¶ Registers double click callback.
This method should be called before calling
UIStyler.Dialog.Show()
orUIStyler.Dialog.RegisterWithUiMenu()
Signature
AddDoubleClickHandler(doubleclickevent, isDialogLaunchingEvent)
Parameters: - doubleclickevent (CallableObject) –
- isDialogLaunchingEvent (bool) –
New in version NX5.0.0.
License requirements: None.
Append¶
-
MultiSelectList.
Append
¶ Appends one or more entries to be inserted into the list
Signature
Append(multiEntries)
Parameters: multiEntries (list of str) – An array of entry names to be inserted into the list. This field is used only when more than one entry are to be inserted into the list. New in version NX5.0.0.
License requirements: None.
DeleteSubitem¶
-
MultiSelectList.
DeleteSubitem
¶ Deletes sub item
Signature
DeleteSubitem(subItemIndex)
Parameters: subItemIndex (int) – Zero-based index of a list entry to be deleted New in version NX5.0.0.
License requirements: None.
Deselect¶
-
MultiSelectList.
Deselect
¶ Requests a list entry to be deselected.
Signature
Deselect(subItemIndex)
Parameters: subItemIndex (int) – Index of the list entry to be deselected. New in version NX5.0.0.
License requirements: None.
Focus¶
-
MultiSelectList.
Focus
¶ Indicates that this dialog item is receiving keyboard focus.
Signature
Focus()
New in version NX5.0.0.
License requirements: None.
GetAllIndicesSelected¶
-
MultiSelectList.
GetAllIndicesSelected
¶ Gets the indices of all selected list entries.
Signature
GetAllIndicesSelected()
Returns: An array of integers for item indices of selected items Return type: list of int New in version NX5.0.0.
License requirements: None.
GetAllNameSelected¶
-
MultiSelectList.
GetAllNameSelected
¶ Gets the names of all selected list entries.
Signature
GetAllNameSelected()
Returns: An array of character strings of selected items Return type: list of str New in version NX5.0.0.
License requirements: None.
GetListItems¶
-
MultiSelectList.
GetListItems
¶ Gets an array of character strings for item names that are used as selectable choices for this dialog item.
Signature
GetListItems()
Returns: An array of character strings for item names Return type: list of str New in version NX5.0.0.
License requirements: None.
InsertSubitems¶
-
MultiSelectList.
InsertSubitems
¶ Signature
InsertSubitems(subitemIndex, multiEntries)
Parameters: - subitemIndex (int) – Sub item index
- multiEntries (list of str) – An array of items to be inserted
New in version NX5.0.0.
License requirements: None.
SetAllSelected¶
-
MultiSelectList.
SetAllSelected
¶ Specifies all list entry to be selected.
Signature
SetAllSelected()
New in version NX5.0.0.
License requirements: None.
SetListItems¶
-
MultiSelectList.
SetListItems
¶ Specifies an array of character strings for item names that are used as selectable choices for this dialog item.
Signature
SetListItems(itemVal)
Parameters: itemVal (list of str) – array of character strings for item names New in version NX5.0.0.
License requirements: None.
SetSelected¶
-
MultiSelectList.
SetSelected
¶ Specifies particular list items to be selected.
Signature
SetSelected(subIndex)
Parameters: subIndex (int) – An index of particular list items to be selected New in version NX5.0.0.
License requirements: None.
ShowSubItem¶
-
MultiSelectList.
ShowSubItem
¶ Requests a list entry to be scrolled up to the first line in the list
Signature
ShowSubItem(subItemIndex)
Parameters: subItemIndex (int) – Zero-based index of a list entry to be scrolled up to the first line of the list. New in version NX5.0.0.
License requirements: None.