IntegerScale Class¶
-
class
NXOpen.UIStyler.
IntegerScale
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a IntegerScale for UI Styler
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ItemValue | Returns or sets |
Sensitivity | Returns or sets the sensitivity of the dialog item. |
Visibility | Returns or sets the visibility of the dialog item. |
Methods¶
Method | Description |
---|---|
AddDragHandler | Registers drag callback. |
AddValueChangedHandler | Registers value change callback. |
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
InitializeAttachment | Returns initialized dialog item attachment information |
IsEqualTo | Equates two styler items |
SetAttachment | Specifies the updated dialog item attachment information |
SetLabels | Specifies the text for the minimum and maximum label. |
SetLimits | Specifies the scale’s maximum and minimum value. |
Property Detail¶
ItemValue¶
-
IntegerScale.
ItemValue
¶ Returns or sets
-------------------------------------
Getter Method
Signature
ItemValue
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ItemValue
Parameters: itemVal (int) – New in version NX5.0.0.
License requirements: None.
Sensitivity¶
-
IntegerScale.
Sensitivity
¶ Returns or sets the sensitivity of the dialog item.
-------------------------------------
Getter Method
Signature
Sensitivity
Returns: TRUE if sensitive, FALSE if insensitive Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sensitivity
Parameters: type (bool) – TRUE if sensitive, FALSE if insensitive New in version NX5.0.0.
License requirements: None.
Visibility¶
-
IntegerScale.
Visibility
¶ Returns or sets the visibility of the dialog item.
-------------------------------------
Getter Method
Signature
Visibility
Returns: TRUE if visible, FALSE if invisible Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility
Parameters: type (bool) – TRUE if visible, FALSE if invisible New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddDragHandler¶
-
IntegerScale.
AddDragHandler
¶ Registers drag callback.
This method should be called before calling
UIStyler.Dialog.Show()
orUIStyler.Dialog.RegisterWithUiMenu()
Signature
AddDragHandler(dragevent, isDialogLaunchingEvent)
Parameters: - dragevent (CallableObject) –
- isDialogLaunchingEvent (bool) –
New in version NX5.0.0.
License requirements: None.
AddValueChangedHandler¶
-
IntegerScale.
AddValueChangedHandler
¶ Registers value change callback.
This method should be called before calling
UIStyler.Dialog.Show()
orUIStyler.Dialog.RegisterWithUiMenu()
Signature
AddValueChangedHandler(valuechangedevent, isDialogLaunchingEvent)
Parameters: - valuechangedevent (CallableObject) – Value changed event
- isDialogLaunchingEvent (bool) – True if launch any dialog else False
New in version NX5.0.0.
License requirements: None.
SetLabels¶
-
IntegerScale.
SetLabels
¶ Specifies the text for the minimum and maximum label.
By default, the system uses the maximum/minimum value as a text label.
Signature
SetLabels(minimumLabel, maximumLabel)
Parameters: - minimumLabel (str) – minimum limit for label
- maximumLabel (str) – maximum limit for label
New in version NX5.0.0.
License requirements: None.