FileOperationData Class¶
-
class
NXOpen.UIStyler.
FileOperationData
¶ Bases:
NXOpen.TransientObject
Represents a FileOperationData for UI Styler
New in version NX5.0.0.
Enumerations¶
FileOperationDataFileOperationState Enumeration | Describes file state |
FileOperationDataFileOperationType Enumeration | Describes file operation |
Property Detail¶
State¶
-
FileOperationData.
State
¶ Returns the state
-------------------------------------
Getter Method
Signature
State
Returns: Return type: NXOpen.UIStyler.FileOperationDataFileOperationState
New in version NX5.0.0.
License requirements: None.
Type¶
-
FileOperationData.
Type
¶ Returns the file operation type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.UIStyler.FileOperationDataFileOperationType
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
FileOperationData.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET or Java, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX5.0.0.
License requirements: None.