FileOperationDataFileOperationType Enumeration¶
NXOpen.UIStyler.FileOperationData.FileOperationType is an alias for NXOpen.UIStyler.FileOperationDataFileOperationType
-
class
NXOpen.UIStyler.
FileOperationDataFileOperationType
¶ Bases:
object
Describes file operation
Enum Members
Enum Member Enum Member Description New New file operation Open Open file operation Save Save file operation SaveAs Save as file operation SaveAll Save all file operation Close Close file operation Quit Quit file operation SaveAndExit Save and Exit file operation ChangePart Chaneg part file operation Execute Execute file operation Reopen Reopen file operation SaveAllAndClose Save all and close file operation SaveAndClose Save and close file operation SaveAsAndClose Save as and close file operation -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-