ButtonLayout Class¶
-
class
NXOpen.UIStyler.
ButtonLayout
¶ Bases:
NXOpen.UIStyler.StylerItem
Represents a Button Layout for UI Styler.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Visibility | Returns or sets the visibility |
Methods¶
Method | Description |
---|---|
AddActivateHandler | Registers activate callback. |
Dispose | Free resources associated with the instance. |
GetItemType | Gets the dialog item type. |
GetSelectedIndexValue | Gets selected index |
GetSensitivity | Gets the sensitivity |
InitializeAttachment | Returns initialized dialog item attachment information |
IsEqualTo | Equates two styler items |
SetAttachment | Specifies the updated dialog item attachment information |
SetDefaultAction | Sets default action |
SetSensitivity | Sets the sensitivity |
Property Detail¶
Visibility¶
-
ButtonLayout.
Visibility
¶ Returns or sets the visibility
-------------------------------------
Getter Method
Signature
Visibility
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Visibility
Parameters: type (bool) – TRUE if visible, FALSE if invisible New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddActivateHandler¶
-
ButtonLayout.
AddActivateHandler
¶ Registers activate callback.
This method should be called before calling
UIStyler.Dialog.Show()
orUIStyler.Dialog.RegisterWithUiMenu()
Signature
AddActivateHandler(activateevent, isDialogLaunchingEvent)
Parameters: - activateevent (CallableObject) – Callback for activate event
- isDialogLaunchingEvent (bool) – TRUE if dialog is going to launch, FALSE if not
New in version NX5.0.0.
License requirements: None.
GetSelectedIndexValue¶
-
ButtonLayout.
GetSelectedIndexValue
¶ Gets selected index
Signature
GetSelectedIndexValue()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
GetSensitivity¶
-
ButtonLayout.
GetSensitivity
¶ Gets the sensitivity
Signature
GetSensitivity()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
SetDefaultAction¶
-
ButtonLayout.
SetDefaultAction
¶ Sets default action
Signature
SetDefaultAction()
New in version NX5.0.0.
License requirements: None.
SetSensitivity¶
-
ButtonLayout.
SetSensitivity
¶ Sets the sensitivity
Signature
SetSensitivity(subitemIndex, type)
Parameters: - subitemIndex (int) – If the entire dialog item should change to the new sensitivity state, set this field to UF_STYLER_NO_SUB_INDEX. If only one subitem should change to the new sensitivity state, set this field to its zero-based index.
- type (bool) – TRUE if sensitive, FALSE if insensitive
New in version NX5.0.0.
License requirements: None.