NXOpen.UF.Ui.Mask Structure¶
NXOpen.UF.Ui.Mask is an alias for NXOpen.UF.UiMask_Struct
-
class
NXOpen.UF.
UiMask_Struct
¶ Bases:
object
Refer to UF_UI_mask_s for documentation.
Fields
NXOpen.UF.UiMask_Struct.ObjectType |
This can be one of the object types that are listed in uf_object_types.h or UF_pseudo_object_type |
NXOpen.UF.UiMask_Struct.ObjectSubtype |
This can either be UF_all_subtype (not with UF_pseudo_object_type), or one of the corresponding supported subtypes of the object type specified. |
NXOpen.UF.UiMask_Struct.SolidType |
This should be named detail_type and is only meaningful for certain object_types like UF_solid_type, UF_feature_type or UF_pseudo_type. |