UF_UI_mask_s (view source)
 
Defined in: uf_ui_types.h
 
Also known as:
 
Overview
fourth CAE detail type


Data Members

object_type
int
This can be one of the object types that are listed in
uf_object_types.h or UF_pseudo_object_type

object_subtype
int
This can either be UF_all_subtype (not with UF_pseudo_object_type),
or one of the corresponding supported subtypes of the object type specified.
This is ignored for certain types like UF_solid_type

solid_type
int
This should be named detail_type and is only meaningful for certain object_types like
UF_solid_type, UF_feature_type or UF_pseudo_type.
This should be set to one of the corresponding detail types
of the object type and object_subtype specified.
This is ignored for UF_all_subtype.