NXOpen.UF.Modl.SmslotData Structure¶
NXOpen.UF.Modl.SmslotData is an alias for NXOpen.UF.ModlSmslotData_Struct
-
class
NXOpen.UF.
ModlSmslotData_Struct
¶ Bases:
object
Refer to UF_MODL_smslot_data_s for documentation.
Fields
NXOpen.UF.ModlSmslotData_Struct.Length |
Length of SMSlot |
NXOpen.UF.ModlSmslotData_Struct.Width |
Width of SMSlot |
NXOpen.UF.ModlSmslotData_Struct.Depth |
Depth of SMSlot. |
NXOpen.UF.ModlSmslotData_Struct.Edge1 |
Tag of the firstoffset edge |
NXOpen.UF.ModlSmslotData_Struct.Offset1 |
Offset distance from first offset edge |
NXOpen.UF.ModlSmslotData_Struct.Edge2 |
Tag of the second offset edge |
NXOpen.UF.ModlSmslotData_Struct.Offset2 |
Offset distance from second offset edge |
NXOpen.UF.ModlSmslotData_Struct.SlotFace |
Tag of the face on which the SMSlot will be placed |
NXOpen.UF.ModlSmslotData_Struct.ThroughFace |
Tag of the facethrough which the Through SMSlot will be created |
NXOpen.UF.ModlSmslotData_Struct.DirMethod |
Method used to determine angle of central axis of the SMSlot. |
NXOpen.UF.ModlSmslotData_Struct.DDatumAxis |
Tag of the datum axis used to determine the angle of the central axis of the SMSlot. |
NXOpen.UF.ModlSmslotData_Struct.DVecDir |
Direction vector used to determine the angle of the central axis of the SMSlot. |
NXOpen.UF.ModlSmslotData_Struct.OrientMethod |
Method used todetermine angle of the orientation along the length of the SMSlot. |
NXOpen.UF.ModlSmslotData_Struct.ODatumAxis |
Tag of the datum axis used to determine the orientation along the length of the SMSlot. |
NXOpen.UF.ModlSmslotData_Struct.OVecDir |
Orientation vector used to determine the orientation along the length of the SMSlot. |
NXOpen.UF.ModlSmslotData_Struct.Type |
Type of SMSlot to be created. |