UF_MODL_smslot_data_s (view source)
Defined in: uf_modl_smd.h
Also known as:
- UF_MODL_smslot_data_t
- UF_MODL_smslot_data_p_t
Overview
The following structure is used when creating, editing, or querying a
sheet metal slot.
Data Members
length [ UF_MAX_EXP_BUFSIZE ]
char
width [ UF_MAX_EXP_BUFSIZE ]
char
depth [ UF_MAX_EXP_BUFSIZE ]
char
edge1
offset1 [ UF_MAX_EXP_BUFSIZE ]
char
edge2
offset2 [ UF_MAX_EXP_BUFSIZE ]
char
slot_face
through_face
dir_method
d_datum_axis
d_vec_dir [ 3 ]
double
orient_method
o_datum_axis
o_vec_dir [ 3 ]
double
type