NXOpen.UF.Modl.SmreliefData Structure

NXOpen.UF.Modl.SmreliefData is an alias for NXOpen.UF.ModlSmreliefData_Struct

class NXOpen.UF.ModlSmreliefData_Struct

Bases: object

Refer to UF_MODL_smrelief_data_s for documentation.

Fields

NXOpen.UF.ModlSmreliefData_Struct.BaseFace Planar face or any face of a flange
NXOpen.UF.ModlSmreliefData_Struct.FirstCornerEdges Edges defining the first corner, should be in the plane of the base face, These edges must intersect.
NXOpen.UF.ModlSmreliefData_Struct.SecondCornerEdges Edges defining the second corner, should be in the plane of the base face, these edges must intersect
NXOpen.UF.ModlSmreliefData_Struct.OffsetCorner Edges defining the third corner, should be in the plane of the base face
NXOpen.UF.ModlSmreliefData_Struct.FirstCornerFilletRadius radius value for first corner fillet . This has to be greater than zero
NXOpen.UF.ModlSmreliefData_Struct.SecondCornerFilletRadius radius value for second corner fillet . This value has to be greater than zero
NXOpen.UF.ModlSmreliefData_Struct.OsCircleRadius radius value for offset corner fillet. This value must be greater than zero
NXOpen.UF.ModlSmreliefData_Struct.OffsetDistance distance by which fillet will be offset inside the body from the offset corner . This value must be greater than or equal to zero and less than offset_corner_fillet_ radius