UF_MODL_smrelief_data_s (view source)
 
Defined in: uf_modl_smd.h
 
Also known as:
 


Data Members

base_face
tag_t
Planar face or any face
of a flange

first_corner_edges [ 2 ]
tag_t
Edges defining the first
corner, should be in the
plane of the base face,
These edges must
intersect.

second_corner_edges [ 2 ]
tag_t
Edges defining the
second corner, should
be in the plane of the
base face, these edges
must intersect

offset_corner [ 3 ]
double
Edges defining the third
corner, should be in
the plane of the base
face

first_corner_fillet_radius
char *
radius value for first
corner fillet .
This has to be greater
than zero

second_corner_fillet_radius
char *
radius value for second
corner fillet .
This value has to be
greater than zero

os_circle_radius
char *
radius value for offset
corner fillet. This
value must be greater
than zero

offset_distance
char *
distance by which fillet
will be offset inside
the body from the
offset corner . This
value must be greater
than or equal to zero
and less than
offset_corner_fillet_
radius