NXOpen.UF.Modl.SmjoggleData Structure¶
NXOpen.UF.Modl.SmjoggleData is an alias for NXOpen.UF.ModlSmjoggleData_Struct
-
class
NXOpen.UF.
ModlSmjoggleData_Struct
¶ Bases:
object
Refer to UF_MODL_smjoggle_data_s for documentation.
Fields
NXOpen.UF.ModlSmjoggleData_Struct.BaseFace |
|
NXOpen.UF.ModlSmjoggleData_Struct.RefFace1 |
|
NXOpen.UF.ModlSmjoggleData_Struct.RefFace2 |
|
NXOpen.UF.ModlSmjoggleData_Struct.TransStartEdge |
Transition start edge tag |
NXOpen.UF.ModlSmjoggleData_Struct.TransEndEdge |
Transition end edge tag |
NXOpen.UF.ModlSmjoggleData_Struct.BaseEdge |
Base_edge tag - in case an edge is ** picked instead of clr points |
NXOpen.UF.ModlSmjoggleData_Struct.PointOnRf1 |
Pick point on ref face1, used to ** infer mat direction, and to identify the ** joggle creation side |
NXOpen.UF.ModlSmjoggleData_Struct.PointOnRf2 |
pick point on ref face2, used to ** infer mat direction, and to identify the ** joggle creation side |
NXOpen.UF.ModlSmjoggleData_Struct.NumClrPts |
No. |
NXOpen.UF.ModlSmjoggleData_Struct.ClrPoint1 |
First clearance point |
NXOpen.UF.ModlSmjoggleData_Struct.ClrPoint2 |
Second Clearance point |
NXOpen.UF.ModlSmjoggleData_Struct.MatDirection |
inside-inside=0 , outside-outside=1 |
NXOpen.UF.ModlSmjoggleData_Struct.ClrDist |
clearance distance |
NXOpen.UF.ModlSmjoggleData_Struct.BendRadius1 |
Ref Face1 - Base Face bend radius |
NXOpen.UF.ModlSmjoggleData_Struct.BendRadius2 |
Ref Face2 - Base Face bend radius |
NXOpen.UF.ModlSmjoggleData_Struct.TransitionRadius |
Ref Face - Trans Face blend radius |
NXOpen.UF.ModlSmjoggleData_Struct.Run |
|
NXOpen.UF.ModlSmjoggleData_Struct.Table |
Use table or not |
NXOpen.UF.ModlSmjoggleData_Struct.EdgeToEdge |
Is joggle of edge_to_edge type? |
NXOpen.UF.ModlSmjoggleData_Struct.MatThickness |
Material thickness |
NXOpen.UF.ModlSmjoggleData_Struct.BendAllowanceFormula |