UF_MODL_smjoggle_data_s (view source)
 
Defined in: uf_modl_smd.h
 
Also known as:
 


Data Members

base_face
tag_t
<I>

ref_face1
tag_t
<I>

ref_face2
tag_t
<I>

trans_start_edge
tag_t
<I> Transition start edge tag

trans_end_edge
tag_t
<I> Transition end edge tag

base_edge
tag_t
<I> Base_edge tag - in case an edge is
picked instead of clr points

point_on_rf1 [ 3 ]
double
<I> Pick point on ref face1, used to
infer mat direction, and to identify the
joggle creation side

point_on_rf2 [ 3 ]
double
<I> pick point on ref face2, used to
infer mat direction, and to identify the
joggle creation side

num_clr_pts
int
No. of clearance points, 1/2

clr_point1 [ 3 ]
double
<I> First clearance point

clr_point2 [ 3 ]
double
<I> Second Clearance point

mat_direction
logical
<I> inside-inside=0 , outside-outside=1

clr_dist
char *
<I> clearance distance

bend_radius1
char *
<I> Ref Face1 - Base Face bend radius

bend_radius2
char *
<I> Ref Face2 - Base Face bend radius

transition_radius
char *
<I> Ref Face - Trans Face blend radius

run
char *
<I>

table
logical
<I> Use table or not

edge_to_edge
logical
<I> Is joggle of edge_to_edge type?

mat_thickness
char *
<I> Material thickness

bend_allowance_formula
char *
<I>