NXOpen.UF.Modl.RipedgeData Structure

NXOpen.UF.Modl.RipedgeData is an alias for NXOpen.UF.ModlRipedgeData_Struct

class NXOpen.UF.ModlRipedgeData_Struct

Bases: object

Refer to UF_MODL_ripedge_data_s for documentation.

Fields

NXOpen.UF.ModlRipedgeData_Struct.NRipedges Number of rip edges
NXOpen.UF.ModlRipedgeData_Struct.Ripedges Array of rip edges
NXOpen.UF.ModlRipedgeData_Struct.AddTangent To add tangent edges or not
NXOpen.UF.ModlRipedgeData_Struct.GapType 0 - Gap, 1 - Offset
NXOpen.UF.ModlRipedgeData_Struct.Gap Gap value Gap type
NXOpen.UF.ModlRipedgeData_Struct.Offset Offset value - Offset type
NXOpen.UF.ModlRipedgeData_Struct.Extension extension value
NXOpen.UF.ModlRipedgeData_Struct.EndCondition 0 - Rectangular, 1 - Obround