UF_MODL_ripedge_data_s (view source)
 
Defined in: uf_modl_smd.h
 
Also known as:
 


Data Members

n_ripedges
int
Number of rip edges

ripedges
tag_p_t
Array of rip edges

add_tangent
logical
To add tangent edges or not

gap_type
int
0 - Gap, 1 - Offset

gap [ UF_MAX_EXP_BUFSIZE ]
char
Gap value Gap type

offset [ UF_MAX_EXP_BUFSIZE ]
char
Offset value - Offset type

extension [ UF_MAX_EXP_BUFSIZE ]
char
extension value

end_condition
int
0 - Rectangular, 1 - Obround