NXOpen.UF.Modl.GflangeOptionsData Structure¶
NXOpen.UF.Modl.GflangeOptionsData is an alias for NXOpen.UF.ModlGflangeOptionsData_Struct
-
class
NXOpen.UF.
ModlGflangeOptionsData_Struct
¶ Bases:
object
Refer to UF_MODL_gflange_options_data_s for documentation.
Fields
NXOpen.UF.ModlGflangeOptionsData_Struct.InferThickness |
TRUE = Thickness derived from target geometry, FALSE = To be given explicitly |
NXOpen.UF.ModlGflangeOptionsData_Struct.InferSpine |
TRUE = System generates spine normal to all section curves. |
NXOpen.UF.ModlGflangeOptionsData_Struct.RValue |
average strain ratio. For homogenous material this value is 1. r_value is used when area_preserve is set to FALSE. |
NXOpen.UF.ModlGflangeOptionsData_Struct.AreaPreserve |
FALSE = Use the above r_value, TRUE = Do not use the r_value, set it to infinite. |
NXOpen.UF.ModlGflangeOptionsData_Struct.Distortion |
|
NXOpen.UF.ModlGflangeOptionsData_Struct.Tolerance |
|
NXOpen.UF.ModlGflangeOptionsData_Struct.MaxSamplePts |
Maximum number of sample points |
NXOpen.UF.ModlGflangeOptionsData_Struct.ContourLines |
Contour Lines |
NXOpen.UF.ModlGflangeOptionsData_Struct.FormBlockLines |
Form Block Lines |
NXOpen.UF.ModlGflangeOptionsData_Struct.MoldLines |
Mold Lines |