UF_MODL_gflange_options_data_s (view source)
 
Defined in: uf_modl_smd.h
 
Also known as:
 


Data Members

infer_thickness
logical
TRUE = Thickness derived from target
geometry,
FALSE = To be given explicitly

infer_spine
logical
TRUE = System generates spine normal to
all section curves.
FALSE = Use bend edge or spine

r_value [ UF_MAX_EXP_BUFSIZE ]
char
average strain ratio.
For homogenous material this
value is 1. r_value is used
when area_preserve is set
to FALSE.

area_preserve
logical
FALSE = Use the above r_value,
TRUE = Do not use the r_value, set
it to infinite.

distortion
UF_MODL_gflange_distort_t
Distortion

tolerance [ UF_MAX_EXP_BUFSIZE ]
char
Tolerance

max_sample_pts [ UF_MAX_EXP_BUFSIZE ]
char
Maximum number of
sample points

contour_lines
logical
Contour Lines

form_block_lines
logical
Form Block Lines

mold_lines
logical
Mold Lines