NXOpen.UF.Modl.EdgeBlendSetbackData Structure

NXOpen.UF.Modl.EdgeBlendSetbackData is an alias for NXOpen.UF.ModlEdgeBlendSetbackData_Struct

class NXOpen.UF.ModlEdgeBlendSetbackData_Struct

Bases: object

Refer to UF_MODL_edge_blend_setback_data_s for documentation.

Fields

NXOpen.UF.ModlEdgeBlendSetbackData_Struct.Edge The edge on which setback distance has to be specified
NXOpen.UF.ModlEdgeBlendSetbackData_Struct.FromStart if true, then the setback is defined at the start vertex. Otherwise, it is defined at the end vertex.
NXOpen.UF.ModlEdgeBlendSetbackData_Struct.Distance Setback distance
NXOpen.UF.ModlEdgeBlendSetbackData_Struct.DistanceExp Expression TAG will only be set during Edit, User can edit the distance string to edit the new value
NXOpen.UF.ModlEdgeBlendSetbackData_Struct.Status When adding Status = 1 and To remove Status = 0