UF_MODL_edge_blend_setback_data_s (view source)
 
Defined in: uf_modl_blends.h
 
Also known as:
 
Overview
Setback Data Structure


Data Members

edge
tag_t
The edge on which setback distance has to be specified

from_start
logical
if true, then the setback is defined at the start vertex.
Otherwise, it is defined at the end vertex.

distance [ UF_MAX_EXP_BUFSIZE ]
char
Setback distance

distance_exp
tag_t
Expression TAG will only be set during Edit, User can edit the
distance string to edit the new value

status
int
When adding Status = 1 and To remove Status = 0