NXOpen.UF.Modl.EdgeBlendSet Structure

NXOpen.UF.Modl.EdgeBlendSet is an alias for NXOpen.UF.ModlEdgeBlendSet_Struct

class NXOpen.UF.ModlEdgeBlendSet_Struct

Bases: object

Refer to UF_MODL_edge_blend_set_s for documentation.

Fields

NXOpen.UF.ModlEdgeBlendSet_Struct.EdgeCollector The edge collector, if this is a NULL_TAG, then the edges will be read from num_edges and edges
NXOpen.UF.ModlEdgeBlendSet_Struct.NumEdges The edges with a constant radius.
NXOpen.UF.ModlEdgeBlendSet_Struct.Edges
NXOpen.UF.ModlEdgeBlendSet_Struct.Radius Radius associated with these edges
NXOpen.UF.ModlEdgeBlendSet_Struct.RadiusExp Expression TAG will only be set during Edit, User can edit the radius string to edit the new value
NXOpen.UF.ModlEdgeBlendSet_Struct.Status When adding Status = 1 and To remove Status = 0