UF_MODL_edge_blend_set_s (view source)
 
Defined in: uf_modl_blends.h
 
Also known as:
 
Overview
Blend Set(Chainset) Data Structure


Data Members

edge_collector
tag_t
The edge collector, if this is a NULL_TAG, then
the edges will be read from num_edges and edges

num_edges
int
The edges with a constant radius. Is honored only
when the edge_collector is NULL_TAG

edges
tag_t*


radius [ UF_MAX_EXP_BUFSIZE ]
char
Radius associated with these edges

radius_exp
tag_t
Expression TAG will only be set during Edit, User can edit the
radius string to edit the new value

status
int
When adding Status = 1 and To remove Status = 0