NXOpen.UF.Modl.BlendPointData Structure¶
NXOpen.UF.Modl.BlendPointData is an alias for NXOpen.UF.ModlBlendPointData_Struct
-
class
NXOpen.UF.
ModlBlendPointData_Struct
¶ Bases:
object
Refer to UF_MODL_blend_point_data_s for documentation.
Fields
NXOpen.UF.ModlBlendPointData_Struct.Radius |
variable radius at a point |
NXOpen.UF.ModlBlendPointData_Struct.Parameter |
parameter at a point Its the percentage of paramter value so can have values ranging from 0.0 to 1.0 |
NXOpen.UF.ModlBlendPointData_Struct.RadiusExp |
Expression TAG will only be set during Edit, User can edit the radius string to edit the new value |
NXOpen.UF.ModlBlendPointData_Struct.Status |
When adding Status = 1 and To remove Status = 0 |