UF_MODL_blend_point_data_s (view source)
 
Defined in: uf_modl_blends.h
 
Also known as:
 
Overview
Point Data for Variable Radius Structure


Data Members

radius [ UF_MAX_EXP_BUFSIZE ]
char
variable radius at a point

parameter
double
parameter at a point Its the percentage of paramter value
so can have values ranging from 0.0 to 1.0

radius_exp
tag_t
Expression TAG will only be set during Edit, User can edit the
radius string to edit the new value

status
int
When adding Status = 1 and To remove Status = 0