SplitInsertBuilder Class¶
-
class
NXOpen.Tooling.
SplitInsertBuilder
¶ Bases:
NXOpen.Builder
Creates split insert builder for progressive die.
No entity is returned. To create a new instance of this class, use
NXOpen.Tooling.ProgressiveDieManager.CreateSplitInsertBuilder()
Default values.
Property Value KeepOriginal 0 RenameComponent 0 New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
KeepOriginal | Returns or sets the keep original toggle value |
RenameComponent | Returns or sets the rename component |
SelectComponent | Returns the select component |
SplittingCurves | Returns the splitting curves |
SplittingDirection | Returns or sets the splitting direction |
Tag | Returns the Tag for this object. |
WizardType | Returns or sets the wizard type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FindLinkedBodyFeatureAndSource | Find linked body feature and source object. |
FindLinkedBodyFeatureAndSourceForAll | Find linked body feature and source object. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetComponentFullName | Suppress child feature. |
GetComponentOrigin | Suppress child feature. |
GetComponentTransform | Suppress child feature. |
GetObject | Returns the object currently being edited by this builder. |
PrepairToSplitInsert | Suppress child feature. |
ReverseTrimAndRelinkSourceAndCreateUDOForAll | Reverse trim direction, relink source, and create udo for all. |
SaveAndGetComponentParent | Suppress child feature. |
SetLinkFeatureAndSourceObject | Set link feature and source object. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
KeepOriginal¶
-
SplitInsertBuilder.
KeepOriginal
¶ Returns or sets the keep original toggle value
-------------------------------------
Getter Method
Signature
KeepOriginal
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepOriginal
Parameters: keepOriginal (bool) – New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
RenameComponent¶
-
SplitInsertBuilder.
RenameComponent
¶ Returns or sets the rename component
-------------------------------------
Getter Method
Signature
RenameComponent
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RenameComponent
Parameters: renameComponent (bool) – New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
SelectComponent¶
-
SplitInsertBuilder.
SelectComponent
¶ Returns the select component
-------------------------------------
Getter Method
Signature
SelectComponent
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX12.0.0.
License requirements: None.
SplittingCurves¶
-
SplitInsertBuilder.
SplittingCurves
¶ Returns the splitting curves
-------------------------------------
Getter Method
Signature
SplittingCurves
Returns: Return type: NXOpen.Section
New in version NX12.0.0.
License requirements: None.
SplittingDirection¶
-
SplitInsertBuilder.
SplittingDirection
¶ Returns or sets the splitting direction
-------------------------------------
Getter Method
Signature
SplittingDirection
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SplittingDirection
Parameters: splittingDirection (bool) – New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
WizardType¶
-
SplitInsertBuilder.
WizardType
¶ Returns or sets the wizard type
-------------------------------------
Getter Method
Signature
WizardType
Returns: Return type: int New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WizardType
Parameters: wizardType (int) – New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
FindLinkedBodyFeatureAndSource¶
-
SplitInsertBuilder.
FindLinkedBodyFeatureAndSource
¶ Find linked body feature and source object.
Signature
FindLinkedBodyFeatureAndSource(featureType, featureNameSubString)
Parameters: - featureType (str) –
- featureNameSubString (str) –
New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
FindLinkedBodyFeatureAndSourceForAll¶
-
SplitInsertBuilder.
FindLinkedBodyFeatureAndSourceForAll
¶ Find linked body feature and source object.
Signature
FindLinkedBodyFeatureAndSourceForAll()
New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
GetComponentFullName¶
-
SplitInsertBuilder.
GetComponentFullName
¶ Suppress child feature.
Signature
GetComponentFullName(componentTag)
Parameters: componentTag ( NXOpen.NXObject
) –Returns: Return type: str New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
GetComponentOrigin¶
-
SplitInsertBuilder.
GetComponentOrigin
¶ Suppress child feature.
Signature
GetComponentOrigin(componentTag)
Parameters: componentTag ( NXOpen.NXObject
) –Returns: Return type: NXOpen.Point3d
New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
GetComponentTransform¶
-
SplitInsertBuilder.
GetComponentTransform
¶ Suppress child feature.
Signature
GetComponentTransform(componentTag)
Parameters: componentTag ( NXOpen.NXObject
) –Returns: Return type: NXOpen.Matrix3x3
New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
PrepairToSplitInsert¶
-
SplitInsertBuilder.
PrepairToSplitInsert
¶ Suppress child feature.
Signature
PrepairToSplitInsert()
New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
ReverseTrimAndRelinkSourceAndCreateUDOForAll¶
-
SplitInsertBuilder.
ReverseTrimAndRelinkSourceAndCreateUDOForAll
¶ Reverse trim direction, relink source, and create udo for all.
Signature
ReverseTrimAndRelinkSourceAndCreateUDOForAll(sourceObjects)
Parameters: sourceObjects (list of NXOpen.NXObject
) –New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
SaveAndGetComponentParent¶
-
SplitInsertBuilder.
SaveAndGetComponentParent
¶ Suppress child feature.
Signature
SaveAndGetComponentParent(componentTag)
Parameters: componentTag ( NXOpen.NXObject
) –Returns: Return type: NXOpen.NXObject
New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
SetLinkFeatureAndSourceObject¶
-
SplitInsertBuilder.
SetLinkFeatureAndSourceObject
¶ Set link feature and source object.
Signature
SetLinkFeatureAndSourceObject()
Returns: Return type: list of NXOpen.NXObject
New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Validate¶
-
SplitInsertBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.