ElectrodeComponentBuilder Class¶
-
class
NXOpen.Tooling.
ElectrodeComponentBuilder
¶ Bases:
NXOpen.Builder
Electrode component builder to install holder and pallet.
To create a new instance of this class, use
NXOpen.Tooling.ElectrodeDesignCollection.CreateComponentBuilder()
Default values.
Property Value ReferPart 0 Rename 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ChuckType | Returns or sets the electrode chuck type. |
ComponentMatrix | Returns or sets the component matrix. |
Face | Returns the face whose center will be the origin of the machine set csys. |
Fixture | Returns the part which is an electrode fixture to be edited. |
MateCsys | Returns or sets the current machine set CSYS. |
Parent | Returns the part which is the assembly parent to install an electrode chuck. |
ReferPart | Returns or sets the option to install a chuck by referring to the template part directly or not. |
ReferenceCenter | Returns or sets the component reference point. |
Rename | Returns or sets the option to use the part name management dialog box or not. |
StandardData | Returns or sets the electrode standard data spraedsheet. |
StandardPart | Returns or sets the electrode standard part to be installed. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
InstallComponentPart | Install a holder or a pallet part. |
SetTemplateDataName | The template data name of holder or pallet. |
SetTemplatePartName | The template part name of holder or pallet. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ElectrodeComponentBuilderChuck Enumeration | Represents the electrode chuck type. |
Property Detail¶
ChuckType¶
-
ElectrodeComponentBuilder.
ChuckType
¶ Returns or sets the electrode chuck type.
-------------------------------------
Getter Method
Signature
ChuckType
Returns: Return type: NXOpen.Tooling.ElectrodeComponentBuilderChuck
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChuckType
Parameters: chuck ( NXOpen.Tooling.ElectrodeComponentBuilderChuck
) –New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
ComponentMatrix¶
-
ElectrodeComponentBuilder.
ComponentMatrix
¶ Returns or sets the component matrix.
-------------------------------------
Getter Method
Signature
ComponentMatrix
Returns: component matrix Return type: NXOpen.Matrix3x3
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ComponentMatrix
Parameters: matrix ( NXOpen.Matrix3x3
) – component matrixNew in version NX12.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Face¶
-
ElectrodeComponentBuilder.
Face
¶ Returns the face whose center will be the origin of the machine set csys.
-------------------------------------
Getter Method
Signature
Face
Returns: Return type: NXOpen.SelectFace
New in version NX8.0.0.
License requirements: None.
Fixture¶
-
ElectrodeComponentBuilder.
Fixture
¶ Returns the part which is an electrode fixture to be edited.
-------------------------------------
Getter Method
Signature
Fixture
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX8.0.0.
License requirements: None.
MateCsys¶
-
ElectrodeComponentBuilder.
MateCsys
¶ Returns or sets the current machine set CSYS.
-------------------------------------
Getter Method
Signature
MateCsys
Returns: Return type: NXOpen.NXObject
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MateCsys
Parameters: csys ( NXOpen.NXObject
) –New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Parent¶
-
ElectrodeComponentBuilder.
Parent
¶ Returns the part which is the assembly parent to install an electrode chuck.
-------------------------------------
Getter Method
Signature
Parent
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX8.0.0.
License requirements: None.
ReferPart¶
-
ElectrodeComponentBuilder.
ReferPart
¶ Returns or sets the option to install a chuck by referring to the template part directly or not.
-------------------------------------
Getter Method
Signature
ReferPart
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferPart
Parameters: referPart (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
ReferenceCenter¶
-
ElectrodeComponentBuilder.
ReferenceCenter
¶ Returns or sets the component reference point.
-------------------------------------
Getter Method
Signature
ReferenceCenter
Returns: component position Return type: NXOpen.Point3d
New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceCenter
Parameters: point ( NXOpen.Point3d
) – component positionNew in version NX12.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Rename¶
-
ElectrodeComponentBuilder.
Rename
¶ Returns or sets the option to use the part name management dialog box or not.
-------------------------------------
Getter Method
Signature
Rename
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Rename
Parameters: rename (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
StandardData¶
-
ElectrodeComponentBuilder.
StandardData
¶ Returns or sets the electrode standard data spraedsheet.
-------------------------------------
Getter Method
Signature
StandardData
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StandardData
Parameters: standardData (str) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
StandardPart¶
-
ElectrodeComponentBuilder.
StandardPart
¶ Returns or sets the electrode standard part to be installed.
-------------------------------------
Getter Method
Signature
StandardPart
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StandardPart
Parameters: standardPart (str) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Method Detail¶
InstallComponentPart¶
-
ElectrodeComponentBuilder.
InstallComponentPart
¶ Install a holder or a pallet part.
Signature
InstallComponentPart(templateData, libraryName, catalogName, classificationName, titleName)
Parameters: - templateData (
NXOpen.Tooling.SpreadsheetData
) – spread sheet data of the standard part - libraryName (str) – library name of the standard part
- catalogName (str) – catalog name of the standard part
- classificationName (str) – classification name of the standard part
- titleName (str) – title name of the standard part
Returns: Return type: New in version NX12.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
- templateData (
SetTemplateDataName¶
-
ElectrodeComponentBuilder.
SetTemplateDataName
¶ The template data name of holder or pallet.
Signature
SetTemplateDataName(templateDataName)
Parameters: templateDataName (str) – New in version NX12.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
SetTemplatePartName¶
-
ElectrodeComponentBuilder.
SetTemplatePartName
¶ The template part name of holder or pallet.
Signature
SetTemplatePartName(templatePartName)
Parameters: templatePartName (str) – New in version NX12.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Validate¶
-
ElectrodeComponentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.