DieEngDieTipBuilder Class¶
-
class
NXOpen.Tooling.
DieEngDieTipBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Die Engineer die tip management builder.
To create a new instance of this class, use
NXOpen.Tooling.AutoDieCollection.CreateDieEngDieTipBuilder()
Default values.
Property Value ChangeTipOrientations 1 ChangeTipOrigin 1 GenerateOutline 1 InheritTip 1 Thickness 0 ThicknessType Uniform WithoutWorkflow 0 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ChangeTipOrientations | Returns or sets the change tip orientations toggle option |
ChangeTipOrigin | Returns or sets the change tip origin |
GenerateOutline | Returns or sets the generate outline toggle option |
InheritTip | Returns or sets the inherit tip toggle option |
Origin | Returns or sets the origin point |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Product | Returns the die tip product sheet body |
ReferenceData | Returns the reference data |
StampingOperation | Returns the stamping operation |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
SyncOrigin | Returns or sets the synchroous origin toggle option |
Tag | Returns the Tag for this object. |
Thickness | Returns or sets the material thickness |
ThicknessType | Returns or sets the thickness type |
WithoutWorkflow | Returns or sets the without workflow toggle option |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
MoreDetails | Callback of button more details |
ObjectProperties | Callback of object properties button |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DieEngDieTipBuilderMaterialThicknessType Enumeration | the material thickness type |
Property Detail¶
ChangeTipOrientations¶
-
DieEngDieTipBuilder.
ChangeTipOrientations
¶ Returns or sets the change tip orientations toggle option
-------------------------------------
Getter Method
Signature
ChangeTipOrientations
Returns: Return type: bool New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
ChangeTipOrientations
Parameters: changeTipOrientations (bool) – New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
ChangeTipOrigin¶
-
DieEngDieTipBuilder.
ChangeTipOrigin
¶ Returns or sets the change tip origin
-------------------------------------
Getter Method
Signature
ChangeTipOrigin
Returns: Return type: bool New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
ChangeTipOrigin
Parameters: changeTipOrigin (bool) – New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GenerateOutline¶
-
DieEngDieTipBuilder.
GenerateOutline
¶ Returns or sets the generate outline toggle option
-------------------------------------
Getter Method
Signature
GenerateOutline
Returns: Return type: bool New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
GenerateOutline
Parameters: generateOutline (bool) – New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
InheritTip¶
-
DieEngDieTipBuilder.
InheritTip
¶ Returns or sets the inherit tip toggle option
-------------------------------------
Getter Method
Signature
InheritTip
Returns: Return type: bool New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
InheritTip
Parameters: inheritTip (bool) – New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Origin¶
-
DieEngDieTipBuilder.
Origin
¶ Returns or sets the origin point
-------------------------------------
Getter Method
Signature
Origin
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
Origin
Parameters: origin ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Product¶
-
DieEngDieTipBuilder.
Product
¶ Returns the die tip product sheet body
-------------------------------------
Getter Method
Signature
Product
Returns: Return type: NXOpen.SelectBody
New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
ReferenceData¶
-
DieEngDieTipBuilder.
ReferenceData
¶ Returns the reference data
-------------------------------------
Getter Method
Signature
ReferenceData
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
StampingOperation¶
-
DieEngDieTipBuilder.
StampingOperation
¶ Returns the stamping operation
-------------------------------------
Getter Method
Signature
StampingOperation
Returns: Return type: NXOpen.SelectNXObject
New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SyncOrigin¶
-
DieEngDieTipBuilder.
SyncOrigin
¶ Returns or sets the synchroous origin toggle option
-------------------------------------
Getter Method
Signature
SyncOrigin
Returns: Return type: int New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
SyncOrigin
Parameters: syncOrigin (int) – New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Thickness¶
-
DieEngDieTipBuilder.
Thickness
¶ Returns or sets the material thickness
-------------------------------------
Getter Method
Signature
Thickness
Returns: Return type: float New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
Thickness
Parameters: thickness (float) – New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
ThicknessType¶
-
DieEngDieTipBuilder.
ThicknessType
¶ Returns or sets the thickness type
-------------------------------------
Getter Method
Signature
ThicknessType
Returns: Return type: NXOpen.Tooling.DieEngDieTipBuilderMaterialThicknessType
New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
ThicknessType
Parameters: thicknessType ( NXOpen.Tooling.DieEngDieTipBuilderMaterialThicknessType
) –New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
WithoutWorkflow¶
-
DieEngDieTipBuilder.
WithoutWorkflow
¶ Returns or sets the without workflow toggle option
-------------------------------------
Getter Method
Signature
WithoutWorkflow
Returns: Return type: bool New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
WithoutWorkflow
Parameters: withoutWorkflow (bool) – New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Method Detail¶
MoreDetails¶
-
DieEngDieTipBuilder.
MoreDetails
¶ Callback of button more details
Signature
MoreDetails()
New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
ObjectProperties¶
-
DieEngDieTipBuilder.
ObjectProperties
¶ Callback of object properties button
Signature
ObjectProperties()
New in version NX11.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Validate¶
-
DieEngDieTipBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.