DieDesDrawPunchBuilder Class¶
-
class
NXOpen.Tooling.
DieDesDrawPunchBuilder
¶ Bases:
NXOpen.Builder
Die Design draw punch management builder, create a draw die punch by selected sheet body, curve and base plane.
To create a new instance of this class, use
NXOpen.Tooling.AutoDieCollection.CreateDieDesDrawPunchBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ApproximateSheetbodyOption | Returns or sets the option to indicate whether to use approximate sheet metal. |
BasePlane | Returns or sets the base plane, which is used for define the base of the punch. |
BaseThickness | Returns or sets the base thickness, which is used for define the base thickness of the die. |
BaseWidth | Returns or sets the base width, which is used for define the base width value of the die. |
BeltThickness | Returns or sets the belt thickness, which is used for define the belt thickness of the punch. |
CoreDrawPunchOption | Returns or sets the option to indicate whether to create core draw punch. |
DeckThickness | Returns or sets the deck thickness, which is used for define the deck thickness of the punch. |
ExactSheetbodyOption | Returns or sets the option to indicate whether to use exact sheet metal. |
FlangeProfile | Returns the flange profile, which is used for user defined flange shape. |
MachiningAllowance | Returns or sets the machining allowance, which is used for define the user machining allowance of the punch. |
MainWallCenterLine | Returns the main wall center line profile, which is used for user defined main wall shape. |
PunchCurve | Returns the punch curve, which is used for wall extrusion. |
ReliefAngle | Returns or sets the relief angle thickness, which is used for define the relief angle of the punch. |
ReliefDistance | Returns or sets the relief distance thickness, which is used for define the relief distance of the punch. |
SheetBody | Returns the sheet body, which is used to trim the punch top face. |
SheetBodyDeck | Returns the inner deck sheet body, which is used for draw punch inner deck face. |
Tag | Returns the Tag for this object. |
TfeatureSet | Returns or sets the feature set tag. |
WallThickness | Returns or sets the wall thickness, which is used for define the wall thickness of the die. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ApproximateSheetbodyOption¶
-
DieDesDrawPunchBuilder.
ApproximateSheetbodyOption
¶ Returns or sets the option to indicate whether to use approximate sheet metal.
-------------------------------------
Getter Method
Signature
ApproximateSheetbodyOption
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApproximateSheetbodyOption
Parameters: approximateSheetbodyOption (bool) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
BasePlane¶
-
DieDesDrawPunchBuilder.
BasePlane
¶ Returns or sets the base plane, which is used for define the base of the punch.
-------------------------------------
Getter Method
Signature
BasePlane
Returns: Return type: NXOpen.Plane
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BasePlane
Parameters: basePlane ( NXOpen.Plane
) –New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
BaseThickness¶
-
DieDesDrawPunchBuilder.
BaseThickness
¶ Returns or sets the base thickness, which is used for define the base thickness of the die.
-------------------------------------
Getter Method
Signature
BaseThickness
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BaseThickness
Parameters: baseThickness (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
BaseWidth¶
-
DieDesDrawPunchBuilder.
BaseWidth
¶ Returns or sets the base width, which is used for define the base width value of the die.
-------------------------------------
Getter Method
Signature
BaseWidth
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BaseWidth
Parameters: baseWidth (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
BeltThickness¶
-
DieDesDrawPunchBuilder.
BeltThickness
¶ Returns or sets the belt thickness, which is used for define the belt thickness of the punch.
-------------------------------------
Getter Method
Signature
BeltThickness
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BeltThickness
Parameters: beltThickness (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
CoreDrawPunchOption¶
-
DieDesDrawPunchBuilder.
CoreDrawPunchOption
¶ Returns or sets the option to indicate whether to create core draw punch.
-------------------------------------
Getter Method
Signature
CoreDrawPunchOption
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoreDrawPunchOption
Parameters: coreDrawPunchOption (bool) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
DeckThickness¶
-
DieDesDrawPunchBuilder.
DeckThickness
¶ Returns or sets the deck thickness, which is used for define the deck thickness of the punch.
-------------------------------------
Getter Method
Signature
DeckThickness
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeckThickness
Parameters: deckThickness (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
ExactSheetbodyOption¶
-
DieDesDrawPunchBuilder.
ExactSheetbodyOption
¶ Returns or sets the option to indicate whether to use exact sheet metal.
This function has been obsoleted, use
Tooling.DieDesDrawPunchBuilder.ApproximateSheetbodyOption()
for substitution.-------------------------------------
Getter Method
Signature
ExactSheetbodyOption
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExactSheetbodyOption
Parameters: exactSheetbodyOption (bool) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
FlangeProfile¶
-
DieDesDrawPunchBuilder.
FlangeProfile
¶ Returns the flange profile, which is used for user defined flange shape.
-------------------------------------
Getter Method
Signature
FlangeProfile
Returns: Return type: NXOpen.Section
New in version NX8.0.0.
License requirements: None.
MachiningAllowance¶
-
DieDesDrawPunchBuilder.
MachiningAllowance
¶ Returns or sets the machining allowance, which is used for define the user machining allowance of the punch.
-------------------------------------
Getter Method
Signature
MachiningAllowance
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MachiningAllowance
Parameters: machiningAllowance (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
MainWallCenterLine¶
-
DieDesDrawPunchBuilder.
MainWallCenterLine
¶ Returns the main wall center line profile, which is used for user defined main wall shape.
-------------------------------------
Getter Method
Signature
MainWallCenterLine
Returns: Return type: NXOpen.Section
New in version NX8.0.0.
License requirements: None.
PunchCurve¶
-
DieDesDrawPunchBuilder.
PunchCurve
¶ Returns the punch curve, which is used for wall extrusion.
-------------------------------------
Getter Method
Signature
PunchCurve
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
ReliefAngle¶
-
DieDesDrawPunchBuilder.
ReliefAngle
¶ Returns or sets the relief angle thickness, which is used for define the relief angle of the punch.
-------------------------------------
Getter Method
Signature
ReliefAngle
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReliefAngle
Parameters: reliefAngle (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
ReliefDistance¶
-
DieDesDrawPunchBuilder.
ReliefDistance
¶ Returns or sets the relief distance thickness, which is used for define the relief distance of the punch.
-------------------------------------
Getter Method
Signature
ReliefDistance
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReliefDistance
Parameters: reliefDistance (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
SheetBody¶
-
DieDesDrawPunchBuilder.
SheetBody
¶ Returns the sheet body, which is used to trim the punch top face.
-------------------------------------
Getter Method
Signature
SheetBody
Returns: Return type: NXOpen.SelectBody
New in version NX8.0.0.
License requirements: None.
SheetBodyDeck¶
-
DieDesDrawPunchBuilder.
SheetBodyDeck
¶ Returns the inner deck sheet body, which is used for draw punch inner deck face.
-------------------------------------
Getter Method
Signature
SheetBodyDeck
Returns: Return type: NXOpen.SelectBody
New in version NX8.0.0.
License requirements: None.
TfeatureSet¶
-
DieDesDrawPunchBuilder.
TfeatureSet
¶ Returns or sets the feature set tag.
-------------------------------------
Getter Method
Signature
TfeatureSet
Returns: Return type: NXOpen.Features.Feature
New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
TfeatureSet
Parameters: tFeatureSet ( NXOpen.Features.Feature
) –New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
WallThickness¶
-
DieDesDrawPunchBuilder.
WallThickness
¶ Returns or sets the wall thickness, which is used for define the wall thickness of the die.
-------------------------------------
Getter Method
Signature
WallThickness
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WallThickness
Parameters: wallThickness (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
Validate¶
-
DieDesDrawPunchBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.