DieDesDrawDieBuilder Class¶
-
class
NXOpen.Tooling.
DieDesDrawDieBuilder
¶ Bases:
NXOpen.Builder
Represents the Die Design draw die management builder, which is to create a draw die by selected sheet body, curve and base plane.
To create a new instance of this class, use
NXOpen.Tooling.AutoDieCollection.CreateDieDesDrawDieBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ApproximateSheetbodyOption | Returns or sets the option to indicate whether to use approximate sheet metal. |
BasePlane | Returns or sets the base plane, which is used for define the base of the die. |
BaseThickness | Returns or sets the base thickness, which is used for define the base thickness of the die. |
BinderEdgeOffset | Returns or sets the binder edge offset, which is used for define the binder edge offset value of the die. |
BlankCurve | Returns the blank curve, which is used for extrusion. |
CoreDrawDieOption | Returns or sets the option to indicate whether to create core draw die. |
DeckEdgeOffset | Returns or sets the deck edge offset, which is used for define the deck edge offset value of the die. |
DeckFlangeThickness | Returns or sets the deck flange thickness, which is used for define the flange thickness of the die. |
DeckThickness | Returns or sets the deck thickness, which is used for define the deck thickness of the die. |
ExactSheetbodyOption | Returns or sets the option to indicate whether to use exact sheet body. |
FlangeCurve | Returns the flange curve, which is used for extrusion. |
FlangeOffset | Returns or sets the flange offset, which is the offset value from projected blank curve to flange curve. |
MachiningAllowance | Returns or sets the machining allowance, which is used for define the user machining allowance of the die. |
PunchCurve | Returns the punch curve, which is used for extrusion. |
SheetBody | Returns the sheet body, which is used to trim the die top face. |
Tag | Returns the Tag for this object. |
TfeatureSet | Returns or sets the feature set tag. |
WallThickness | Returns or sets the wall thickness, which is used for define the wall thickness of the die. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ApproximateSheetbodyOption¶
-
DieDesDrawDieBuilder.
ApproximateSheetbodyOption
¶ Returns or sets the option to indicate whether to use approximate sheet metal.
-------------------------------------
Getter Method
Signature
ApproximateSheetbodyOption
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApproximateSheetbodyOption
Parameters: approximateSheetbodyOption (bool) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
BasePlane¶
-
DieDesDrawDieBuilder.
BasePlane
¶ Returns or sets the base plane, which is used for define the base of the die.
-------------------------------------
Getter Method
Signature
BasePlane
Returns: Return type: NXOpen.Plane
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BasePlane
Parameters: basePlane ( NXOpen.Plane
) –New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
BaseThickness¶
-
DieDesDrawDieBuilder.
BaseThickness
¶ Returns or sets the base thickness, which is used for define the base thickness of the die.
-------------------------------------
Getter Method
Signature
BaseThickness
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BaseThickness
Parameters: baseThickness (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
BinderEdgeOffset¶
-
DieDesDrawDieBuilder.
BinderEdgeOffset
¶ Returns or sets the binder edge offset, which is used for define the binder edge offset value of the die.
-------------------------------------
Getter Method
Signature
BinderEdgeOffset
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BinderEdgeOffset
Parameters: binderEdgeOffset (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
BlankCurve¶
-
DieDesDrawDieBuilder.
BlankCurve
¶ Returns the blank curve, which is used for extrusion.
-------------------------------------
Getter Method
Signature
BlankCurve
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
CoreDrawDieOption¶
-
DieDesDrawDieBuilder.
CoreDrawDieOption
¶ Returns or sets the option to indicate whether to create core draw die.
-------------------------------------
Getter Method
Signature
CoreDrawDieOption
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoreDrawDieOption
Parameters: coreDrawDieOption (bool) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
DeckEdgeOffset¶
-
DieDesDrawDieBuilder.
DeckEdgeOffset
¶ Returns or sets the deck edge offset, which is used for define the deck edge offset value of the die.
-------------------------------------
Getter Method
Signature
DeckEdgeOffset
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeckEdgeOffset
Parameters: deckEdgeOffset (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
DeckFlangeThickness¶
-
DieDesDrawDieBuilder.
DeckFlangeThickness
¶ Returns or sets the deck flange thickness, which is used for define the flange thickness of the die.
-------------------------------------
Getter Method
Signature
DeckFlangeThickness
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeckFlangeThickness
Parameters: deckFlangeThickness (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
DeckThickness¶
-
DieDesDrawDieBuilder.
DeckThickness
¶ Returns or sets the deck thickness, which is used for define the deck thickness of the die.
-------------------------------------
Getter Method
Signature
DeckThickness
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeckThickness
Parameters: deckThickness (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
ExactSheetbodyOption¶
-
DieDesDrawDieBuilder.
ExactSheetbodyOption
¶ Returns or sets the option to indicate whether to use exact sheet body.
This function has been obsoleted, use
Tooling.DieDesDrawDieBuilder.ApproximateSheetbodyOption()
for substitution.-------------------------------------
Getter Method
Signature
ExactSheetbodyOption
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExactSheetbodyOption
Parameters: exactSheetbodyOption (bool) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
FlangeCurve¶
-
DieDesDrawDieBuilder.
FlangeCurve
¶ Returns the flange curve, which is used for extrusion.
-------------------------------------
Getter Method
Signature
FlangeCurve
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
FlangeOffset¶
-
DieDesDrawDieBuilder.
FlangeOffset
¶ Returns or sets the flange offset, which is the offset value from projected blank curve to flange curve.
-------------------------------------
Getter Method
Signature
FlangeOffset
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlangeOffset
Parameters: flangeOffset (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
MachiningAllowance¶
-
DieDesDrawDieBuilder.
MachiningAllowance
¶ Returns or sets the machining allowance, which is used for define the user machining allowance of the die.
-------------------------------------
Getter Method
Signature
MachiningAllowance
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MachiningAllowance
Parameters: machiningAllowance (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
PunchCurve¶
-
DieDesDrawDieBuilder.
PunchCurve
¶ Returns the punch curve, which is used for extrusion.
-------------------------------------
Getter Method
Signature
PunchCurve
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
SheetBody¶
-
DieDesDrawDieBuilder.
SheetBody
¶ Returns the sheet body, which is used to trim the die top face.
-------------------------------------
Getter Method
Signature
SheetBody
Returns: Return type: NXOpen.SelectBody
New in version NX8.0.0.
License requirements: None.
TfeatureSet¶
-
DieDesDrawDieBuilder.
TfeatureSet
¶ Returns or sets the feature set tag.
-------------------------------------
Getter Method
Signature
TfeatureSet
Returns: Return type: NXOpen.Features.Feature
New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
TfeatureSet
Parameters: tFeatureSet ( NXOpen.Features.Feature
) –New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
WallThickness¶
-
DieDesDrawDieBuilder.
WallThickness
¶ Returns or sets the wall thickness, which is used for define the wall thickness of the die.
-------------------------------------
Getter Method
Signature
WallThickness
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WallThickness
Parameters: wallThickness (float) – New in version NX8.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
Validate¶
-
DieDesDrawDieBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.