ColorExpressionsBuilder Class¶
-
class
NXOpen.Tooling.
ColorExpressionsBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.ColorExpressionsBuilder
builder.To create a new instance of this class, use
NXOpen.Tooling.MoldwizardManager.CreateColorExpressionsBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
ColorName | Returns or sets the color name |
ColorPicker | Returns or sets the color picker |
SelectFaces | Returns the solid faces selected by user |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
BlockCurrentUDO | Block current udo |
Commit | Commits any edits that have been applied to the builder. |
DeleteCurrentUDO | Delete current udo |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetCurrentUDO | Select current udo |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ColorName¶
-
ColorExpressionsBuilder.
ColorName
¶ Returns or sets the color name
-------------------------------------
Getter Method
Signature
ColorName
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorName
Parameters: colorName (str) – New in version NX12.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
ColorPicker¶
-
ColorExpressionsBuilder.
ColorPicker
¶ Returns or sets the color picker
-------------------------------------
Getter Method
Signature
ColorPicker
Returns: Return type: Id New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorPicker
Parameters: colorPicker (Id) – New in version NX12.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SelectFaces¶
-
ColorExpressionsBuilder.
SelectFaces
¶ Returns the solid faces selected by user
-------------------------------------
Getter Method
Signature
SelectFaces
Returns: Return type: NXOpen.ScCollector
New in version NX12.0.0.
License requirements: None.
Method Detail¶
BlockCurrentUDO¶
-
ColorExpressionsBuilder.
BlockCurrentUDO
¶ Block current udo
Signature
BlockCurrentUDO(blocked)
Parameters: blocked (bool) – New in version NX12.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
DeleteCurrentUDO¶
-
ColorExpressionsBuilder.
DeleteCurrentUDO
¶ Delete current udo
Signature
DeleteCurrentUDO()
New in version NX12.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SetCurrentUDO¶
-
ColorExpressionsBuilder.
SetCurrentUDO
¶ Select current udo
Signature
SetCurrentUDO(udo)
Parameters: udo ( NXOpen.UserDefinedObjects.UserDefinedObject
) – The udo objectNew in version NX12.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Validate¶
-
ColorExpressionsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.