NXOpen.ShipDesign Package¶
Classes¶
ApplicationUtils Class | Represents Generator which wrap the ship api for china |
GeneralArrangementManager Class | Represents the interface for General Arrangement classes |
Generator Class | Represents Generator which wrap the ship api for china |
Navigator Class | Represents the interface for navigator action classes |
NavigatorCollection Class | Represents the interface for navigator action classes |
NavigatorNode Class | Represents the interface for navigator view classes |
NavigatorView Class | Represents the interface for navigator view classes |
ShipNavigatorNodeBuilder Class | Represents the ship navigator node builder to add or edit ship navigator node. |
ShipNavigatorRoot Class | Represents the interface for ship navigator root classes. |
ShipSession Class | Represents Ship session |
Enumerations¶
GeneratorClashType Enumeration | Clash status to indicate to show space position relation between two bodies 1. |
ShipNavigatorNodeBuilderNodeTypes Enumeration | Settings to indicate the type of ship navigator node. |