ShipNavigatorNodeBuilderNodeTypes Enumeration¶
NXOpen.ShipDesign.ShipNavigatorNodeBuilder.NodeTypes is an alias for NXOpen.ShipDesign.ShipNavigatorNodeBuilderNodeTypes
-
class
NXOpen.ShipDesign.
ShipNavigatorNodeBuilderNodeTypes
¶ Bases:
object
Settings to indicate the type of ship navigator node.
Enum Members
Enum Member Enum Member Description Object The object node type. Part The part node type. Container The container node type. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-