ShapeSearchBuilder Class¶
-
class
NXOpen.ShapeSearch.
ShapeSearchBuilder
¶ Bases:
NXOpen.Builder
This class provides the methods to execute shape search and get the searched results.
The operation that this builder supports has three types: (set by
ShapeSearch.ShapeSearchBuilder.SearchType()
)- Search by attributes.
ShapeSearch.ShapeSearchBuilder.SetInputAttributesName()
ShapeSearch.ShapeSearchBuilder.SetInputAttributesFilter()
- Search by body combined attributes with shape similarity and shape size condition. Support multiple bodies.
ShapeSearch.ShapeSearchBuilder.InputBody()
ShapeSearch.ShapeSearchBuilder.SetInputAttributesName()
ShapeSearch.ShapeSearchBuilder.SetInputAttributesFilter()
ShapeSearch.ShapeSearchBuilder.SearchShapeSimilarity()
ShapeSearch.ShapeSearchBuilder.SearchShapeSize()
ShapeSearch.ShapeSearchBuilder.UseCustomShapeSize()
ShapeSearch.ShapeSearchBuilder.CustomShapeSizeLowerLimit()
ShapeSearch.ShapeSearchBuilder.CustomShapeSizeUpperLimit()
- Search by part combined attributes with shape similarity and shape size condition. Support loaded part, OS part, Teamcenter part and component.
ShapeSearch.ShapeSearchBuilder.InputPart()
ShapeSearch.ShapeSearchBuilder.SetInputAttributesName()
ShapeSearch.ShapeSearchBuilder.SetInputAttributesFilter()
ShapeSearch.ShapeSearchBuilder.ReferenceSetName()
ShapeSearch.ShapeSearchBuilder.SearchShapeSimilarity()
ShapeSearch.ShapeSearchBuilder.SearchShapeSize()
ShapeSearch.ShapeSearchBuilder.UseCustomShapeSize()
ShapeSearch.ShapeSearchBuilder.CustomShapeSizeLowerLimit()
ShapeSearch.ShapeSearchBuilder.CustomShapeSizeUpperLimit()
When initialize builder, we will load all saved searches from work directory and add them to search list. You can implement
ShapeSearch.ShapeSearchBuilder.ExecuteSearch()
to run the saved search.After define the search criteria, function
ShapeSearch.ShapeSearchBuilder.ExecuteSearch()
can search the shape from database and return the searched results count and error message if fails. The search is specified by ‘searchName’ parameter.The method
ShapeSearch.ShapeSearchBuilder.GetResults()
can get the specified results from database. The range of results is specified by the parameters ‘startResultId’ and ‘endResultId’, the search is specified by ‘searchName’ parameter.The method
ShapeSearch.ShapeSearchBuilder.OpenResultPart()
can open the selected result part of the specified search. The result is specified by ‘resultId’ parameter, the search is specified by ‘searchName’ parameter.To create a new instance of this class, use
NXOpen.ShapeSearch.SearchManager.CreateShapeSearchBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CustomShapeSizeLowerLimit | Returns or sets the custom shape size lower limit to be set for search. |
CustomShapeSizeUpperLimit | Returns or sets the custom shape size upper limit to be set for search. |
InputBody | Returns the input body to be searched |
InputPart | Returns or sets the input part to be searched |
ReferenceSetName | Returns or sets the part reference set name to be set for search |
SearchShapeSimilarity | Returns or sets the shape similarity to be set for search |
SearchShapeSize | Returns or sets the shape size to be set for search. |
SearchType | Returns or sets the search type |
Tag | Returns the Tag for this object. |
UseCustomShapeSize | Returns or sets the use custom shape size to control use shape size option or custom shape size |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
ExecuteSearch | Execute new search or saved search and output error message if error. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetInputAttributesFilter | The input attributes filter to be searched |
GetInputAttributesName | The input attributes name to be searched |
GetObject | Returns the object currently being edited by this builder. |
GetResults | Get specified search results from database. |
OpenResultPart | Open the searched result part. |
SetInputAttributesFilter | The input attributes filter to be searched |
SetInputAttributesName | The input attributes name to be searched |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ShapeSearchBuilderOpenPartType Enumeration | The open part type enum |
ShapeSearchBuilderSearchByType Enumeration | The search type enum |
ShapeSearchBuilderShapeSimilarity Enumeration | The search shape similarity enum |
ShapeSearchBuilderShapeSize Enumeration | The search shape size enum |
Property Detail¶
CustomShapeSizeLowerLimit¶
-
ShapeSearchBuilder.
CustomShapeSizeLowerLimit
¶ Returns or sets the custom shape size lower limit to be set for search.
It is used only when use custom shape size is true. It must be greater than zero and less than upper limit.
-------------------------------------
Getter Method
Signature
CustomShapeSizeLowerLimit
Returns: Return type: int New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
-------------------------------------
Setter Method
Signature
CustomShapeSizeLowerLimit
Parameters: customShapeSizeLowerLimit (int) – New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
CustomShapeSizeUpperLimit¶
-
ShapeSearchBuilder.
CustomShapeSizeUpperLimit
¶ Returns or sets the custom shape size upper limit to be set for search.
It is used only when use custom shape size is true. It must be greater than lower limit.
-------------------------------------
Getter Method
Signature
CustomShapeSizeUpperLimit
Returns: Return type: int New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
-------------------------------------
Setter Method
Signature
CustomShapeSizeUpperLimit
Parameters: customShapeSizeUpperLimit (int) – New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
InputBody¶
-
ShapeSearchBuilder.
InputBody
¶ Returns the input body to be searched
-------------------------------------
Getter Method
Signature
InputBody
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
InputPart¶
-
ShapeSearchBuilder.
InputPart
¶ Returns or sets the input part to be searched
-------------------------------------
Getter Method
Signature
InputPart
Returns: Return type: str New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
-------------------------------------
Setter Method
Signature
InputPart
Parameters: inputPart (str) – New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
ReferenceSetName¶
-
ShapeSearchBuilder.
ReferenceSetName
¶ Returns or sets the part reference set name to be set for search
-------------------------------------
Getter Method
Signature
ReferenceSetName
Returns: Return type: str New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
-------------------------------------
Setter Method
Signature
ReferenceSetName
Parameters: referenceSetName (str) – New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
SearchShapeSimilarity¶
-
ShapeSearchBuilder.
SearchShapeSimilarity
¶ Returns or sets the shape similarity to be set for search
-------------------------------------
Getter Method
Signature
SearchShapeSimilarity
Returns: Return type: NXOpen.ShapeSearch.ShapeSearchBuilderShapeSimilarity
New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
-------------------------------------
Setter Method
Signature
SearchShapeSimilarity
Parameters: searchShapeSimilarity ( NXOpen.ShapeSearch.ShapeSearchBuilderShapeSimilarity
) –New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
SearchShapeSize¶
-
ShapeSearchBuilder.
SearchShapeSize
¶ Returns or sets the shape size to be set for search.
It is used only when use custom shape size is false.
-------------------------------------
Getter Method
Signature
SearchShapeSize
Returns: Return type: NXOpen.ShapeSearch.ShapeSearchBuilderShapeSize
New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
-------------------------------------
Setter Method
Signature
SearchShapeSize
Parameters: searchShapeSize ( NXOpen.ShapeSearch.ShapeSearchBuilderShapeSize
) –New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
SearchType¶
-
ShapeSearchBuilder.
SearchType
¶ Returns or sets the search type
-------------------------------------
Getter Method
Signature
SearchType
Returns: Return type: NXOpen.ShapeSearch.ShapeSearchBuilderSearchByType
New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
-------------------------------------
Setter Method
Signature
SearchType
Parameters: searchType ( NXOpen.ShapeSearch.ShapeSearchBuilderSearchByType
) –New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
UseCustomShapeSize¶
-
ShapeSearchBuilder.
UseCustomShapeSize
¶ Returns or sets the use custom shape size to control use shape size option or custom shape size
-------------------------------------
Getter Method
Signature
UseCustomShapeSize
Returns: Return type: bool New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
-------------------------------------
Setter Method
Signature
UseCustomShapeSize
Parameters: useCustomShapeSize (bool) – New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
Method Detail¶
ExecuteSearch¶
-
ShapeSearchBuilder.
ExecuteSearch
¶ Execute new search or saved search and output error message if error.
Signature
ExecuteSearch(isNew, searchName)
Parameters: - isNew (bool) – True is executing new search, False is executing saved search
- searchName (str) – Search name
Returns: a tuple
Return type: A tuple consisting of (nTotalResults, errorMessage) nTotalResults is a int. Search result total number errorMessage is a str. Search error message
New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
GetInputAttributesFilter¶
-
ShapeSearchBuilder.
GetInputAttributesFilter
¶ The input attributes filter to be searched
Signature
GetInputAttributesFilter()
Returns: Return type: list of str New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
GetInputAttributesName¶
-
ShapeSearchBuilder.
GetInputAttributesName
¶ The input attributes name to be searched
Signature
GetInputAttributesName()
Returns: Return type: list of str New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
GetResults¶
-
ShapeSearchBuilder.
GetResults
¶ Get specified search results from database.
Signature
GetResults(searchName, startResultId, endResultId)
Parameters: - searchName (str) – Search name
- startResultId (int) – Start result id
- endResultId (int) – End result id
New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
OpenResultPart¶
-
ShapeSearchBuilder.
OpenResultPart
¶ Open the searched result part.
Signature
OpenResultPart(openPartType, searchName, resultId)
Parameters: - openPartType (
NXOpen.ShapeSearch.ShapeSearchBuilderOpenPartType
) – Open part type - searchName (str) – Search name
- resultId (int) – Result id
New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
- openPartType (
SetInputAttributesFilter¶
-
ShapeSearchBuilder.
SetInputAttributesFilter
¶ The input attributes filter to be searched
Signature
SetInputAttributesFilter(inputAttributesFilter)
Parameters: inputAttributesFilter (list of str) – Search attributes filter New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
SetInputAttributesName¶
-
ShapeSearchBuilder.
SetInputAttributesName
¶ The input attributes name to be searched
Signature
SetInputAttributesName(inputAttributesName)
Parameters: inputAttributesName (list of str) – Search attributes Name New in version NX6.0.0.
License requirements: shape_search (“Shape Search”)
Validate¶
-
ShapeSearchBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.