ShapeSearchBuilderShapeSize Enumeration¶
NXOpen.ShapeSearch.ShapeSearchBuilder.ShapeSize is an alias for NXOpen.ShapeSearch.ShapeSearchBuilderShapeSize
-
class
NXOpen.ShapeSearch.
ShapeSearchBuilderShapeSize
¶ Bases:
object
The search shape size enum
Enum Members
Enum Member Enum Member Description P90P110 search with shape size 90%-110% condition P80P120 search with shape size 80%-120% condition P70P130 search with shape size 70%-130% condition P50P200 search with shape size 50%-200% condition P25P400 search with shape size 25%-400% condition -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-