SaveOptions Class¶
-
class
NXOpen.
SaveOptions
¶ Bases:
object
Contains accessor methods for all part save options that follow the session.
See
NXOpen.PartSaveOptions
for those part save options that are specific to a particular part. To obtain an instance of this class, refer toNXOpen.PartCollection
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
FamilyDefaultDirectory | Returns or sets the option that specifies the directory in which you want to file part family members. |
TrueShapeData | Returns or sets the option indicating whether to generate data for true shape filtering (.ts files) |
VisualizationData | Returns or sets the option indicating whether to generate Teamcenter Visualization .jt files when a part is saved |
Methods¶
Property Detail¶
FamilyDefaultDirectory¶
-
SaveOptions.
FamilyDefaultDirectory
¶ Returns or sets the option that specifies the directory in which you want to file part family members.
Note that setting this property will have no effect while running in NX Manager mode.
-------------------------------------
Getter Method
Signature
FamilyDefaultDirectory
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FamilyDefaultDirectory
Parameters: dir (str) – New in version NX3.0.0.
License requirements: None.
TrueShapeData¶
-
SaveOptions.
TrueShapeData
¶ Returns or sets the option indicating whether to generate data for true shape filtering (.ts files)
-------------------------------------
Getter Method
Signature
TrueShapeData
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrueShapeData
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
VisualizationData¶
-
SaveOptions.
VisualizationData
¶ Returns or sets the option indicating whether to generate Teamcenter Visualization .jt files when a part is saved
-------------------------------------
Getter Method
Signature
VisualizationData
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizationData
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.