PartSaveOptions Class¶
-
class
NXOpen.
PartSaveOptions
¶ Bases:
object
Contains accessor methods for all part save options that follow the part.
See
SaveOptions
for those part save options that are not specific to a particular part. To obtain an instance of this class, refer toNXOpen.BasePart
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Annotation3dData | Returns or sets the option indicating whether to generate 3D Annotation data and store in NX part Quick Access Folder when you save the part file |
CompressPart | Returns or sets the option indicating whether solid data within part files will be compressed as it is saved to disk |
DrawingCgmData | Returns or sets the option indicating whether to generate the CGM data and store it in the QAF when you save the part file |
GenerateWeightData | Returns or sets the option indicating whether the weight and other mass properties of a part will be updated and saved when the part is saved |
PatternDataToSave | Returns or sets the option indicating how pattern data will be saved while saving a part |
Methods¶
Enumerations¶
PartSaveOptionsPatternData Enumeration | Options for specifying how pattern data should be saved while saving a part |
Property Detail¶
Annotation3dData¶
-
PartSaveOptions.
Annotation3dData
¶ Returns or sets the option indicating whether to generate 3D Annotation data and store in NX part Quick Access Folder when you save the part file
-------------------------------------
Getter Method
Signature
Annotation3dData
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Annotation3dData
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
CompressPart¶
-
PartSaveOptions.
CompressPart
¶ Returns or sets the option indicating whether solid data within part files will be compressed as it is saved to disk
-------------------------------------
Getter Method
Signature
CompressPart
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CompressPart
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
DrawingCgmData¶
-
PartSaveOptions.
DrawingCgmData
¶ Returns or sets the option indicating whether to generate the CGM data and store it in the QAF when you save the part file
-------------------------------------
Getter Method
Signature
DrawingCgmData
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DrawingCgmData
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
GenerateWeightData¶
-
PartSaveOptions.
GenerateWeightData
¶ Returns or sets the option indicating whether the weight and other mass properties of a part will be updated and saved when the part is saved
-------------------------------------
Getter Method
Signature
GenerateWeightData
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GenerateWeightData
Parameters: option (bool) – New in version NX3.0.0.
License requirements: None.
PatternDataToSave¶
-
PartSaveOptions.
PatternDataToSave
¶ Returns or sets the option indicating how pattern data will be saved while saving a part
-------------------------------------
Getter Method
Signature
PatternDataToSave
Returns: Return type: NXOpen.PartSaveOptionsPatternData
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PatternDataToSave
Parameters: option ( NXOpen.PartSaveOptionsPatternData
) –New in version NX3.0.0.
License requirements: None.