PostConfiguratorManager Class¶
-
class
NXOpen.SIM.PostConfigurator.
PostConfiguratorManager
¶ Bases:
object
Represents Post Configurator Manager
Use
NXOpen.Session.PostConfiguratorManager()
to get the instance of this class.New in version NX10.0.3.
Methods¶
Method | Description |
---|---|
CreateCreationPostBuilder | Creates a NXOpen.SIM.PostConfigurator.CreationPostBuilder object |
CreatePostConfiguratorBuilder | Creates a NXOpen.SIM.PostConfigurator.PostConfiguratorBuilder object |
Method Detail¶
CreateCreationPostBuilder¶
-
PostConfiguratorManager.
CreateCreationPostBuilder
¶ Creates a
NXOpen.SIM.PostConfigurator.CreationPostBuilder
objectSignature
CreateCreationPostBuilder()
Returns: The new creation post builder Return type: NXOpen.SIM.PostConfigurator.CreationPostBuilder
New in version NX10.0.3.
License requirements: nx_post_config_full (“NX Post Configurator”) OR nx_post_config_adv (“NX Post Configurator”)
CreatePostConfiguratorBuilder¶
-
PostConfiguratorManager.
CreatePostConfiguratorBuilder
¶ Creates a
NXOpen.SIM.PostConfigurator.PostConfiguratorBuilder
objectSignature
CreatePostConfiguratorBuilder(postProcessorFilename)
Parameters: postProcessorFilename (str) – the post processor filename Returns: The new post configurator builder Return type: NXOpen.SIM.PostConfigurator.PostConfiguratorBuilder
New in version NX10.0.3.
License requirements: nx_post_config_full (“NX Post Configurator”) OR nx_post_config_adv (“NX Post Configurator”)