PostConfiguratorBuilder Class¶
-
class
NXOpen.SIM.PostConfigurator.
PostConfiguratorBuilder
¶ Bases:
NXOpen.Builder
This class is used to create a post configurator builder.
Calling
Builder.Commit()
on this builder will only return None.To create a new instance of this class, use
NXOpen.SIM.PostConfigurator.PostConfiguratorManager.CreatePostConfiguratorBuilder()
New in version NX10.0.3.
Properties¶
Property | Description |
---|---|
DateValue | Returns the date value. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EncryptPostConfiguratorFiles | Encrypts a post processor with Sold-To ID and expiration date. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
Reset | Resets the post configurator data. |
SaveAs | Saves the post configurator data in different name. |
ShowChanges | Shows the post configurator data changes in the listing window. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DateValue¶
-
PostConfiguratorBuilder.
DateValue
¶ Returns the date value.
The Date object will contain the value for expiration date.
-------------------------------------
Getter Method
Signature
DateValue
Returns: the date value Return type: NXOpen.DateBuilder
New in version NX10.0.3.
License requirements: None.
Method Detail¶
EncryptPostConfiguratorFiles¶
-
PostConfiguratorBuilder.
EncryptPostConfiguratorFiles
¶ Encrypts a post processor with Sold-To ID and expiration date.
Signature
EncryptPostConfiguratorFiles(soldToID, expirationDate)
Parameters: - soldToID (str) – the sold to id
- expirationDate (str) – the expiration date
New in version NX10.0.3.
License requirements: nx_post_config_full (“NX Post Configurator”) OR nx_post_config_adv (“NX Post Configurator”)
Reset¶
-
PostConfiguratorBuilder.
Reset
¶ Resets the post configurator data.
Signature
Reset()
New in version NX10.0.3.
License requirements: nx_post_config_full (“NX Post Configurator”) OR nx_post_config_adv (“NX Post Configurator”)
SaveAs¶
-
PostConfiguratorBuilder.
SaveAs
¶ Saves the post configurator data in different name.
Signature
SaveAs(postprocessorName, outputDirectory)
Parameters: - postprocessorName (str) – the postprocessor name
- outputDirectory (str) – the output directory
New in version NX11.0.1.
License requirements: nx_post_config_full (“NX Post Configurator”) OR nx_post_config_adv (“NX Post Configurator”)
ShowChanges¶
-
PostConfiguratorBuilder.
ShowChanges
¶ Shows the post configurator data changes in the listing window.
Signature
ShowChanges()
New in version NX10.0.3.
License requirements: nx_post_config_full (“NX Post Configurator”) OR nx_post_config_adv (“NX Post Configurator”)
Validate¶
-
PostConfiguratorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.