KinematicJunctionBuilder Class¶
-
class
NXOpen.SIM.
KinematicJunctionBuilder
¶ Bases:
NXOpen.Builder
Represents the SimKimJunctionBuilder class object
Use the
NXOpen.SIM.KinematicConfigurator
class to create a KinematicJunctionBuilder object.New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Classification | Returns or sets the classification of the junction |
Csys | Returns or sets the CSYS associated with the junction |
Name | Returns or sets the kim junction’s name |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateDefaultCsys | Create the default CSYS based on WCS |
CreateTooltipCsys | Create the tooltip CSYS |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
IsMachineZero | Test if this is a machine zero junction |
IsToolMount | Test if the junction is a tool mount junctions |
IsToolTip | Test if the junction is a tool tip junctions |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
KinematicJunctionBuilderSystemClass Enumeration | The junction system classes |
Property Detail¶
Classification¶
-
KinematicJunctionBuilder.
Classification
¶ Returns or sets the classification of the junction
-------------------------------------
Getter Method
Signature
Classification
Returns: the classification of the junction Return type: NXOpen.SIM.KinematicJunctionBuilderSystemClass
New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”) OR resource_manager_nx (“Teamcenter Resource Manager”)
-------------------------------------
Setter Method
Signature
Classification
Parameters: jctClass ( NXOpen.SIM.KinematicJunctionBuilderSystemClass
) – the classification of the junctionNew in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”) OR resource_manager_nx (“Teamcenter Resource Manager”)
Csys¶
-
KinematicJunctionBuilder.
Csys
¶ Returns or sets the CSYS associated with the junction
-------------------------------------
Getter Method
Signature
Csys
Returns: the csys Return type: NXOpen.CartesianCoordinateSystem
New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”) OR resource_manager_nx (“Teamcenter Resource Manager”)
-------------------------------------
Setter Method
Signature
Csys
Parameters: csys ( NXOpen.CartesianCoordinateSystem
) – the csysNew in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”) OR resource_manager_nx (“Teamcenter Resource Manager”)
Name¶
-
KinematicJunctionBuilder.
Name
¶ Returns or sets the kim junction’s name
-------------------------------------
Getter Method
Signature
Name
Returns: The junction’s name Return type: str New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – the junction’s new name New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”) OR resource_manager_nx (“Teamcenter Resource Manager”)
Method Detail¶
CreateDefaultCsys¶
-
KinematicJunctionBuilder.
CreateDefaultCsys
¶ Create the default CSYS based on WCS
Signature
CreateDefaultCsys()
Returns: the default csys Return type: NXOpen.CartesianCoordinateSystem
New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”) OR resource_manager_nx (“Teamcenter Resource Manager”)
CreateTooltipCsys¶
-
KinematicJunctionBuilder.
CreateTooltipCsys
¶ Create the tooltip CSYS
Signature
CreateTooltipCsys()
Returns: the tooltip csys Return type: NXOpen.CartesianCoordinateSystem
New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
IsMachineZero¶
-
KinematicJunctionBuilder.
IsMachineZero
¶ Test if this is a machine zero junction
Signature
IsMachineZero()
Returns: true if it is the machine zero junction Return type: bool New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”)
IsToolMount¶
-
KinematicJunctionBuilder.
IsToolMount
¶ Test if the junction is a tool mount junctions
Signature
IsToolMount()
Returns: true if it is a tool mount junction Return type: bool New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”) OR resource_manager_nx (“Teamcenter Resource Manager”)
IsToolTip¶
-
KinematicJunctionBuilder.
IsToolTip
¶ Test if the junction is a tool tip junctions
Signature
IsToolTip()
Returns: true if it is a tool tip junction Return type: bool New in version NX7.5.0.
License requirements: ug_isv_full (“Full functionality for Integrated Simulation and Verification”) OR nx_isv_mtb (“Machine Tool Builder”) OR resource_manager_nx (“Teamcenter Resource Manager”)
Validate¶
-
KinematicJunctionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.