KinematicJunctionBuilderSystemClass Enumeration¶
NXOpen.SIM.KinematicJunctionBuilder.SystemClass is an alias for NXOpen.SIM.KinematicJunctionBuilderSystemClass
-
class
NXOpen.SIM.
KinematicJunctionBuilderSystemClass
¶ Bases:
object
The junction system classes
Enum Members
Enum Member Enum Member Description NotSet no specal class Mount a mounting junction MachineZero the machine zero junction ToolZero the tool mounting point ToolTip The tool tip junction LatheWpZx Lathe Work Plane Z/X LatheWpXy Lathe Work Plane X/Y -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-