IsvControlPanelBuilderSingleStepType Enumeration¶
NXOpen.SIM.IsvControlPanelBuilder.SingleStepType is an alias for NXOpen.SIM.IsvControlPanelBuilderSingleStepType
-
class
NXOpen.SIM.
IsvControlPanelBuilderSingleStepType
¶ Bases:
object
The Single Step type that used in :py:class:` NXOpen.SIM.IsvControlPanelBuilderVisualizationType.MachineCodeSimulateMtd < NXOpen.SIM.IsvControlPanelBuilderVisualizationType>` or :py:class:` NXOpen.SIM.IsvControlPanelBuilderVisualizationType.ToolPathSimulation < NXOpen.SIM.IsvControlPanelBuilderVisualizationType>` simulation mode. The following
NXOpen.SIM.IsvControlPanelBuilderSingleStepType
members are removed in NX10.0.2: - StepOut - StepIn - Display Replacement: Use the followingNXOpen.SIM.IsvControlPanelBuilderSingleStepModeType
member instead: - :py:class:` NXOpen.SIM.IsvControlPanelBuilderSingleStepModeType.StepOut < NXOpen.SIM.IsvControlPanelBuilderSingleStepModeType>` - :py:class:` NXOpen.SIM.IsvControlPanelBuilderSingleStepModeType.StepIn < NXOpen.SIM.IsvControlPanelBuilderSingleStepModeType>` - :py:class:` NXOpen.SIM.IsvControlPanelBuilderSingleStepModeType.DisplayUpdate < NXOpen.SIM.IsvControlPanelBuilderSingleStepModeType>`Enum Members
Enum Member Enum Member Description Block Block Move Move Event Event -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-