IsvControlPanelBuilderSingleStepModeType Enumeration¶
NXOpen.SIM.IsvControlPanelBuilder.SingleStepModeType is an alias for NXOpen.SIM.IsvControlPanelBuilderSingleStepModeType
-
class
NXOpen.SIM.
IsvControlPanelBuilderSingleStepModeType
¶ Bases:
object
The Single Step Mode type that used in :py:class:` NXOpen.SIM.IsvControlPanelBuilderVisualizationType.MachineCodeSimulateCse < NXOpen.SIM.IsvControlPanelBuilderVisualizationType>` simulation mode.
Enum Members
Enum Member Enum Member Description StepIn Step In StepOver Step Over StepOut Step Out DisplayUpdate Display -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-