Wire Class¶
-
class
NXOpen.Routing.
Wire
¶ Bases:
NXOpen.NXObject
,NXOpen.Routing.IPath
The Routing Wire object is the set of information needed to define * a ROUTE_wire.
Creator not available in KF.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
ControlPointEnd | Returns or sets the end ControlPoint for an IPath object. |
ControlPointStart | Returns or sets the start ControlPoint for an IPath object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddSegmentsToList | Adds segment(s) to an IPath object. |
CreateAttributeIterator | Create an attribute iterator |
DelSegmentsFromList | Removes segment(s) from the IPath object. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSegmentList | Returns the list of all of the segments contained in the IPath |
GetSegments | Returns the segments for the wire. |
GetStock | Returns the stocks for the wire. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
ControlPointEnd¶
-
Wire.
ControlPointEnd
¶ Returns or sets the end ControlPoint for an IPath object.
-------------------------------------
Getter Method
Signature
ControlPointEnd
Returns: end ControlPoint for the IPath object Return type: NXOpen.Routing.ControlPoint
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ControlPointEnd
Parameters: end ( NXOpen.Routing.ControlPoint
) – end ControlPoint for the IPath objectNew in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
ControlPointStart¶
-
Wire.
ControlPointStart
¶ Returns or sets the start ControlPoint for an IPath object.
-------------------------------------
Getter Method
Signature
ControlPointStart
Returns: start ControlPoint for the IPath object Return type: NXOpen.Routing.ControlPoint
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ControlPointStart
Parameters: start ( NXOpen.Routing.ControlPoint
) – start ControlPoint for the IPath objectNew in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
IsOccurrence¶
-
Wire.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Wire.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
Wire.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Wire.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Wire.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
Wire.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
AddSegmentsToList¶
-
Wire.
AddSegmentsToList
¶ Adds segment(s) to an IPath object.
Signature
AddSegmentsToList(objs)
Parameters: objs (list of NXOpen.Routing.ISegment
) – list of segments that are to be addedNew in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
DelSegmentsFromList¶
-
Wire.
DelSegmentsFromList
¶ Removes segment(s) from the IPath object.
Signature
DelSegmentsFromList(objs)
Parameters: objs (list of NXOpen.Routing.ISegment
) – list of segments that are to be deletedNew in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
FindObject¶
-
Wire.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetSegmentList¶
-
Wire.
GetSegmentList
¶ Returns the list of all of the segments contained in the IPath
Signature
GetSegmentList()
Returns: list of all of the segments in this IPath object Return type: list of NXOpen.Routing.ISegment
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetSegments¶
-
Wire.
GetSegments
¶ Returns the segments for the wire.
Signature
GetSegments()
Returns: Return type: list of NXOpen.Routing.ISegment
New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetStock¶
-
Wire.
GetStock
¶ Returns the stocks for the wire.
Signature
GetStock()
Returns: Return type: list of NXOpen.Routing.Stock
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Print¶
-
Wire.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
Wire.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.