PlaceElbowsBuilder Class¶
-
class
NXOpen.Routing.
PlaceElbowsBuilder
¶ Bases:
NXOpen.Builder
Class PlaceElbowsBuilder
To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateRoutingPlaceElbowsBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
AttributeHolder | Returns the attribute holder for elbow placement |
SelectRoutingObjects | Returns the route object collector builder for placing elbows |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
PlaceMultipleElbows | Place Multiple Elbows |
SetAttributeHolder | Set the Attribute Holder |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AttributeHolder¶
-
PlaceElbowsBuilder.
AttributeHolder
¶ Returns the attribute holder for elbow placement
-------------------------------------
Getter Method
Signature
AttributeHolder
Returns: Return type: NXOpen.Routing.AttributeHolder
New in version NX12.0.0.
License requirements: routing_pipetube (“Routing Piping and Tubing”)
SelectRoutingObjects¶
-
PlaceElbowsBuilder.
SelectRoutingObjects
¶ Returns the route object collector builder for placing elbows
-------------------------------------
Getter Method
Signature
SelectRoutingObjects
Returns: Return type: NXOpen.Routing.RouteObjectCollector
New in version NX12.0.0.
License requirements: routing_pipetube (“Routing Piping and Tubing”)
Method Detail¶
PlaceMultipleElbows¶
-
PlaceElbowsBuilder.
PlaceMultipleElbows
¶ Place Multiple Elbows
Signature
PlaceMultipleElbows(jaCharx, refSet, layer, layerOption, overstockFlag, optionalCharx, requiredCharx)
Parameters: - jaCharx (
NXOpen.Routing.CharacteristicList
) – - refSet (str) –
- layer (int) –
- layerOption (int) –
- overstockFlag (bool) –
- optionalCharx (
NXOpen.Routing.CharacteristicList
) – Optional Charx to apply. - requiredCharx (
NXOpen.Routing.CharacteristicList
) – Required Charx to apply.
New in version NX12.0.0.
License requirements: routing_pipetube (“Routing Piping and Tubing”)
- jaCharx (
SetAttributeHolder¶
-
PlaceElbowsBuilder.
SetAttributeHolder
¶ Set the Attribute Holder
Signature
SetAttributeHolder(attributeHolder)
Parameters: attributeHolder ( NXOpen.Routing.AttributeHolder
) – Object to hold template attributesNew in version NX12.0.0.
License requirements: routing_pipetube (“Routing Piping and Tubing”)
Validate¶
-
PlaceElbowsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.