FittingOverstockBuilder Class¶
-
class
NXOpen.Routing.
FittingOverstockBuilder
¶ Bases:
NXOpen.Builder
Builder for creating or editing
NXOpen.Routing.FittingOverstock
objects.To create a new instance of this class, use
NXOpen.Routing.RouteManager.CreateFittingOverstockBuilder()
Default values.
Property Value FaceTrimMethod TrimPlane New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
FaceTrimMethod | Returns or sets the NXOpen.Routing.FittingOverstockBuilderTrimMethod |
Faces | Returns the faces to apply overstock to. |
FirstPlane | Returns or sets the first trimming plane |
OverstockSettings | Returns or sets the stock settings for overstock assignment. |
RoutingParts | Returns the qualifed routing parts to apply overstock to. |
SecondPlane | Returns or sets the second trimming plane |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FittingOverstockBuilderTrimMethod Enumeration | Trimming option. |
FittingOverstockBuilderTypes Enumeration | Overstock application method. |
Property Detail¶
FaceTrimMethod¶
-
FittingOverstockBuilder.
FaceTrimMethod
¶ Returns or sets the
NXOpen.Routing.FittingOverstockBuilderTrimMethod
-------------------------------------
Getter Method
Signature
FaceTrimMethod
Returns: Return type: NXOpen.Routing.FittingOverstockBuilderTrimMethod
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
FaceTrimMethod
Parameters: faceTrimMethod ( NXOpen.Routing.FittingOverstockBuilderTrimMethod
) –New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Faces¶
-
FittingOverstockBuilder.
Faces
¶ Returns the faces to apply overstock to.
-------------------------------------
Getter Method
Signature
Faces
Returns: Return type: NXOpen.SelectFaceList
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FirstPlane¶
-
FittingOverstockBuilder.
FirstPlane
¶ Returns or sets the first trimming plane
-------------------------------------
Getter Method
Signature
FirstPlane
Returns: Return type: NXOpen.Plane
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
FirstPlane
Parameters: firstPlane ( NXOpen.Plane
) –New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
OverstockSettings¶
-
FittingOverstockBuilder.
OverstockSettings
¶ Returns or sets the stock settings for overstock assignment.
-------------------------------------
Getter Method
Signature
OverstockSettings
Returns: Return type: NXOpen.Routing.PathStockBuilder
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
OverstockSettings
Parameters: stockBuilder ( NXOpen.Routing.PathStockBuilder
) –New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
RoutingParts¶
-
FittingOverstockBuilder.
RoutingParts
¶ Returns the qualifed routing parts to apply overstock to.
-------------------------------------
Getter Method
Signature
RoutingParts
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SecondPlane¶
-
FittingOverstockBuilder.
SecondPlane
¶ Returns or sets the second trimming plane
-------------------------------------
Getter Method
Signature
SecondPlane
Returns: Return type: NXOpen.Plane
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
SecondPlane
Parameters: secondPlane ( NXOpen.Plane
) –New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Type¶
-
FittingOverstockBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Routing.FittingOverstockBuilderTypes
New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Routing.FittingOverstockBuilderTypes
) –New in version NX7.5.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Method Detail¶
Validate¶
-
FittingOverstockBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.